<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックUnable to Flash or Debug</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1476884#M14406</link>
    <description>&lt;P&gt;Hello i´m working with the FRDM-K32L3A6 Freedom Development Board,&lt;/P&gt;&lt;P&gt;i just wanted to use some GPIO Pins but i´ve inadverently programmed J7[6] and J7[4] as GPIO Input/Outputs, now i´m unable to flash the board again. I´ve set everything back like it was before, tried to flash the hello world example, tried to use the gui flash tool, made an mass erase, activate sysresreq. Nothing helps there´s always this error message:&lt;/P&gt;&lt;P&gt;Executing flash operation 'Resurrect locked Kinetis device' (Resurrect locked Kinetis device) - Mon Jun 20 16:40:38 CEST 2022&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v11.5 (Dec 16 2021 12:38:31 - crt_emu_cm_redlink.exe build 2)&lt;BR /&gt;( 0) Reading remote configuration&lt;BR /&gt;Wc(03). No cache support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.5 (Dec 16 2021 12:38:31 - crt_emu_cm_redlink build 2)&lt;BR /&gt;Found chip XML file in C:/MCUXpresso_Workspace/frdmk32l3a6_hello_world_demo_cm4/Debug\K32L3A60xxx.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) reports:&lt;BR /&gt;'Ee(42). Could not connect to core.'&lt;BR /&gt;Retrying...&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;============= SCRIPT: K32L3Aconnect.scp =============&lt;BR /&gt;K32L3A M4 Connect Script&lt;BR /&gt;Connecting to Probe Index = 1&lt;BR /&gt;Error: Probe not connected&lt;BR /&gt;Error: Wire Ack Fault - target connected?&lt;BR /&gt;Assert NRESET&lt;BR /&gt;Reset pin state: 00&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;Power up Debug&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;No Debug Power&lt;BR /&gt;============= END SCRIPT ============================&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What can i do to reset the board and to flash it again. I think theres a problem because these pins are something for SWD.&lt;/P&gt;&lt;P&gt;Thanks for you´re help.&lt;/P&gt;</description>
    <pubDate>Mon, 20 Jun 2022 14:49:18 GMT</pubDate>
    <dc:creator>Kolibri</dc:creator>
    <dc:date>2022-06-20T14:49:18Z</dc:date>
    <item>
      <title>Unable to Flash or Debug</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1476884#M14406</link>
      <description>&lt;P&gt;Hello i´m working with the FRDM-K32L3A6 Freedom Development Board,&lt;/P&gt;&lt;P&gt;i just wanted to use some GPIO Pins but i´ve inadverently programmed J7[6] and J7[4] as GPIO Input/Outputs, now i´m unable to flash the board again. I´ve set everything back like it was before, tried to flash the hello world example, tried to use the gui flash tool, made an mass erase, activate sysresreq. Nothing helps there´s always this error message:&lt;/P&gt;&lt;P&gt;Executing flash operation 'Resurrect locked Kinetis device' (Resurrect locked Kinetis device) - Mon Jun 20 16:40:38 CEST 2022&lt;BR /&gt;Checking MCU info...&lt;BR /&gt;Scanning for targets...&lt;BR /&gt;Executing flash action...&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v11.5 (Dec 16 2021 12:38:31 - crt_emu_cm_redlink.exe build 2)&lt;BR /&gt;( 0) Reading remote configuration&lt;BR /&gt;Wc(03). No cache support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.5 (Dec 16 2021 12:38:31 - crt_emu_cm_redlink build 2)&lt;BR /&gt;Found chip XML file in C:/MCUXpresso_Workspace/frdmk32l3a6_hello_world_demo_cm4/Debug\K32L3A60xxx.xml&lt;BR /&gt;( 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) reports:&lt;BR /&gt;'Ee(42). Could not connect to core.'&lt;BR /&gt;Retrying...&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;============= SCRIPT: K32L3Aconnect.scp =============&lt;BR /&gt;K32L3A M4 Connect Script&lt;BR /&gt;Connecting to Probe Index = 1&lt;BR /&gt;Error: Probe not connected&lt;BR /&gt;Error: Wire Ack Fault - target connected?&lt;BR /&gt;Assert NRESET&lt;BR /&gt;Reset pin state: 00&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;Power up Debug&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;Error: Wire not connected&lt;BR /&gt;No Debug Power&lt;BR /&gt;============= END SCRIPT ============================&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What can i do to reset the board and to flash it again. I think theres a problem because these pins are something for SWD.&lt;/P&gt;&lt;P&gt;Thanks for you´re help.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 14:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1476884#M14406</guid>
      <dc:creator>Kolibri</dc:creator>
      <dc:date>2022-06-20T14:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Flash or Debug</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1477555#M14412</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199147"&gt;@Kolibri&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing great.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please try to :&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;1 disconnect your board.&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;2 Press (and maintain pressed) SW2.&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;3 Connect board.&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;4 Release SW2.&lt;/P&gt;
&lt;P class="lia-indent-padding-left-30px"&gt;5 Attempt to debug or program.&lt;/P&gt;
&lt;P&gt;SW2 is connected to the default BOOT_pin of the MCU. If during boot process the BOOT_pin is sampled low the&amp;nbsp; ROM bootloader will be executed by default, instead your application. Thus we have the chance to regain debug access.&lt;/P&gt;
&lt;P&gt;Please let me know your results.&lt;/P&gt;
&lt;P&gt;All the best,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Diego.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jun 2022 15:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1477555#M14412</guid>
      <dc:creator>diego_charles</dc:creator>
      <dc:date>2022-06-21T15:29:03Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Flash or Debug</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1478074#M14421</link>
      <description>&lt;P&gt;Hi diego_charles,&lt;/P&gt;&lt;P&gt;Thanks for the quick reply, it worked! I am able to flash and debug it again.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jun 2022 09:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Unable-to-Flash-or-Debug/m-p/1478074#M14421</guid>
      <dc:creator>Kolibri</dc:creator>
      <dc:date>2022-06-22T09:01:51Z</dc:date>
    </item>
  </channel>
</rss>