<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5744P Interrupt controller - TIMER in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474500#M14364</link>
    <description>&lt;P&gt;Are you referring to this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="INTC2.PNG" style="width: 680px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183484i5CFF51B7AE208EF1/image-size/large?v=v2&amp;amp;px=999" role="button" title="INTC2.PNG" alt="INTC2.PNG" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Anyway after reading your comment, I disabled all FCCU faults and only enabled INTC_MONITOR0, inserted timeout error on IRQ_0 and board is still resetting...&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 13:44:33 GMT</pubDate>
    <dc:creator>Veber</dc:creator>
    <dc:date>2022-06-15T13:44:33Z</dc:date>
    <item>
      <title>MPC5744P Interrupt controller - TIMER</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1473794#M14350</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am working on Interrupt control monitor and there are three IRQs that are monitored. The monitor mode is set to EOI (see the attached picture). In that mode if IRQ latency exceeds that is set in LAT register, error should be signaled, but in the whole reference manual it doesn't says where it will be signaled. Can someone help me with this?&lt;BR /&gt;&lt;BR /&gt;In my case if the IRQ exceeds the latency then INTC_MONITOR0 in FCCU resets my board, even though I set register to no reset reaction.&lt;BR /&gt;&lt;BR /&gt;So if someone can explain me where will the error be signaled I would be very thankful.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 17:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1473794#M14350</guid>
      <dc:creator>Veber</dc:creator>
      <dc:date>2022-06-14T17:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P Interrupt controller - TIMER</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474190#M14357</link>
      <description>&lt;P&gt;Hi, it goes over FCCU. If you don't have enabled reset reaction to this fault, but you have enabled another one, it means also FOSU is active and it may reset the device if FCCU interrupt is not handled on time. Have you checked MC_RGM_DES? F_FFRR indicated FOSU reset.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1655275979823.png" style="width: 767px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183424i4052A32B1E6331B0/image-dimensions/767x652?v=v2" width="767" height="652" role="button" title="davidtosenovjan_0-1655275979823.png" alt="davidtosenovjan_0-1655275979823.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 07:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474190#M14357</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-06-15T07:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P Interrupt controller - TIMER</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474195#M14358</link>
      <description>&lt;P&gt;In the past I made example for FOSU fault injection, but on different MCU that does not have RGM module. But FCCU works more or less same way.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-FCCU-FOSU-error-injection-GHS714/ta-p/1112102" target="_blank"&gt;https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-FCCU-FOSU-error-injection-GHS714/ta-p/1112102&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 07:09:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474195#M14358</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-06-15T07:09:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P Interrupt controller - TIMER</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474500#M14364</link>
      <description>&lt;P&gt;Are you referring to this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="INTC2.PNG" style="width: 680px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183484i5CFF51B7AE208EF1/image-size/large?v=v2&amp;amp;px=999" role="button" title="INTC2.PNG" alt="INTC2.PNG" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Anyway after reading your comment, I disabled all FCCU faults and only enabled INTC_MONITOR0, inserted timeout error on IRQ_0 and board is still resetting...&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 13:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1474500#M14364</guid>
      <dc:creator>Veber</dc:creator>
      <dc:date>2022-06-15T13:44:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P Interrupt controller - TIMER</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1475122#M14372</link>
      <description>&lt;P&gt;Yes, I am referring to this&lt;/P&gt;
&lt;P&gt;Enabling of any fault reaction enables FOSU counter. You just need to clear the fault before ALARM period expires.&lt;/P&gt;
&lt;P&gt;Pay attention to following appnote:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN5284.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5284.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 07:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1475122#M14372</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2022-06-16T07:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P Interrupt controller - TIMER</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1481058#M14484</link>
      <description>&lt;P&gt;Thank you. The problem is solved! &lt;LI-EMOJI id="lia_grinning-face-with-smiling-eyes" title=":grinning_face_with_smiling_eyes:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 08:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC5744P-Interrupt-controller-TIMER/m-p/1481058#M14484</guid>
      <dc:creator>Veber</dc:creator>
      <dc:date>2022-06-28T08:46:33Z</dc:date>
    </item>
  </channel>
</rss>