<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックAccess to post processing source</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Access-to-post-processing-source/m-p/1447155#M13831</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I see that the postprocessing module supplied with eIQ Auto is a compiled library. I want to make use of the output tensor from the object detection demo, but the module does not provide access to the final detections- it only makes a function available "ShowBoxesAndScores", which writes to the console. Is there any call available for me to get I can get direct access to the final detections?&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Rob&lt;/P&gt;</description>
    <pubDate>Thu, 21 Apr 2022 10:01:45 GMT</pubDate>
    <dc:creator>RobShand</dc:creator>
    <dc:date>2022-04-21T10:01:45Z</dc:date>
    <item>
      <title>Access to post processing source</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Access-to-post-processing-source/m-p/1447155#M13831</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I see that the postprocessing module supplied with eIQ Auto is a compiled library. I want to make use of the output tensor from the object detection demo, but the module does not provide access to the final detections- it only makes a function available "ShowBoxesAndScores", which writes to the console. Is there any call available for me to get I can get direct access to the final detections?&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;/P&gt;&lt;P&gt;Rob&lt;/P&gt;</description>
      <pubDate>Thu, 21 Apr 2022 10:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Access-to-post-processing-source/m-p/1447155#M13831</guid>
      <dc:creator>RobShand</dc:creator>
      <dc:date>2022-04-21T10:01:45Z</dc:date>
    </item>
  </channel>
</rss>