<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC8536DS Baord Sleep mode due to 10Ω Resistive load connected in the system? in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8536DS-Baord-Sleep-mode-due-to-10%E2%84%A6-Resistive-load-connected/m-p/180911#M1315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale support Solution :&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&lt;FONT color="#ff0000"&gt;"1) Dummy loads in the Calamary Developmen System are required because of low power consumption of the DS board alone - i.e. when no aditional cards are inserted into PCI Express, Extender and PCI slots. In this case stable operation of the PSU (ANTEC TRUEPOWER TRIO 550) is ensured by the +5V and +12V dummy loads (DALE RH-50W)."&lt;/FONT&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2009 11:45:56 GMT</pubDate>
    <dc:creator>AshishAgarwal</dc:creator>
    <dc:date>2009-05-18T11:45:56Z</dc:date>
    <item>
      <title>MPC8536DS Baord Sleep mode due to 10Ω Resistive load connected in the system?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8536DS-Baord-Sleep-mode-due-to-10%E2%84%A6-Resistive-load-connected/m-p/180910#M1314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know this can be silly question.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am usiing MPC8536DS system baught from Freescale.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;firstly i was able to do my stuff over this system before, now a days due to some customiztion needed on the board desgin i deaattached the motherboard and the SMPS(PSU) from the Mounted CPU Box.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I dismounted theall the wires of chasis power, reset and LED wires.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i booted the system now, it goes in the sleep mode every time i boot it in approx 4-5 secs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;I tried lot of things lastly i review all the work and trced there were two 10Ω resistive loads connected with in the chasis of system. so when i connected those too the system works fine &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;though it worked for me but i am still not clear about why those two resistive loads are needed there.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff"&gt;&lt;IMG border="0" src="file:/C:/DOCUME%7E1/t079903/LOCALS%7E1/Temp/moz-screenshot.jpg" /&gt;resistive loads&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;IMG alt="Resistive Load Looks liks this " border="0" height="103" src="http://www.sphere.bc.ca/test/loads/dale-rer75f6r81r-tiny.jpg" width="250" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or they can view by &lt;A href="http://www.sphere.bc.ca/test/loads.html" rel="nofollow" target="_blank"&gt;CLICK HERE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the rarting written over there is&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;"DALE RH-50W&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;10Ω 1% MEXICO No829"&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason for asking this : newly designed customized board Hw going in sleep mode all the time.&amp;nbsp; (even after coneenting the same resistive laods too)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;If anyone can clear me what the purpose of those Resistive loads it may be a great help for me.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2009 18:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8536DS-Baord-Sleep-mode-due-to-10%E2%84%A6-Resistive-load-connected/m-p/180910#M1314</guid>
      <dc:creator>AshishAgarwal</dc:creator>
      <dc:date>2009-05-13T18:04:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8536DS Baord Sleep mode due to 10Ω Resistive load connected in the system?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8536DS-Baord-Sleep-mode-due-to-10%E2%84%A6-Resistive-load-connected/m-p/180911#M1315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale support Solution :&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&lt;FONT color="#ff0000"&gt;"1) Dummy loads in the Calamary Developmen System are required because of low power consumption of the DS board alone - i.e. when no aditional cards are inserted into PCI Express, Extender and PCI slots. In this case stable operation of the PSU (ANTEC TRUEPOWER TRIO 550) is ensured by the +5V and +12V dummy loads (DALE RH-50W)."&lt;/FONT&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2009 11:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8536DS-Baord-Sleep-mode-due-to-10%E2%84%A6-Resistive-load-connected/m-p/180911#M1315</guid>
      <dc:creator>AshishAgarwal</dc:creator>
      <dc:date>2009-05-18T11:45:56Z</dc:date>
    </item>
  </channel>
</rss>