<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPN7462 with bluetooth module</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PN7462-with-bluetooth-module/m-p/1397329#M12954</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;We have a project the PN7462. This device can be connected to the computer interface and work as a mobile at the same time. We can't use USB and Uart at the same time because of the HIF module(In this case the compiler doesn't allow it). We use it for LCD with full SPI interface. We solved it using I2C to Uart converter. We communicate with the bluetooth module over UART.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can u suggest a bluetooth module for these functions,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regardas,&lt;/P&gt;</description>
    <pubDate>Tue, 11 Jan 2022 10:33:08 GMT</pubDate>
    <dc:creator>kralsemo06</dc:creator>
    <dc:date>2022-01-11T10:33:08Z</dc:date>
    <item>
      <title>PN7462 with bluetooth module</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7462-with-bluetooth-module/m-p/1397329#M12954</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;We have a project the PN7462. This device can be connected to the computer interface and work as a mobile at the same time. We can't use USB and Uart at the same time because of the HIF module(In this case the compiler doesn't allow it). We use it for LCD with full SPI interface. We solved it using I2C to Uart converter. We communicate with the bluetooth module over UART.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can u suggest a bluetooth module for these functions,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regardas,&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jan 2022 10:33:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7462-with-bluetooth-module/m-p/1397329#M12954</guid>
      <dc:creator>kralsemo06</dc:creator>
      <dc:date>2022-01-11T10:33:08Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 with bluetooth module</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7462-with-bluetooth-module/m-p/1397698#M12961</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192192"&gt;@kralsemo06&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt; We communicate with the bluetooth module over UART. Can u suggest a bluetooth module for these functions&lt;BR /&gt;What's the function of the bluetooth module expect to UART interface? Eg. Audio transfer or command to control simple device like switch or light?&lt;BR /&gt;If Audio. Please refer to the IW416 EVK board as the link.&lt;BR /&gt;URL:&lt;A href="https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth/aw-am510-evaluation-board:AW-AM510-USD" target="_blank"&gt;https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth/aw-am510-evaluation-board:AW-AM510-USD&lt;/A&gt;&lt;BR /&gt;If switch or light control. Please refer to the QN9090 module as the link.&lt;BR /&gt;URL:&lt;A href="https://www.nxp.com/products/wireless/bluetooth-low-energy/qn9090dk-development-platform-for-qn9090-30t-wireless-mcus:QN9090-DK006" target="_blank"&gt;https://www.nxp.com/products/wireless/bluetooth-low-energy/qn9090dk-development-platform-for-qn9090-30t-wireless-mcus:QN9090-DK006&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 02:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7462-with-bluetooth-module/m-p/1397698#M12961</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2022-01-12T02:18:19Z</dc:date>
    </item>
  </channel>
</rss>