<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC8555CDS board does not boot 2.6 linux from BPS CD in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179868#M1287</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Paul,&lt;BR /&gt;&lt;BR /&gt;Thanks for the answer.&lt;BR /&gt;I believe you are right about versions. I tried the oldest BSP that contains linux 2.6, which is&amp;nbsp; 20050408. The linux from this iso image boots OK!&lt;BR /&gt;So I use an 'old' linux and the uboot and rootfs of the latest BSP.&lt;BR /&gt;&lt;BR /&gt;Rob&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2008 18:36:46 GMT</pubDate>
    <dc:creator>robthales</dc:creator>
    <dc:date>2008-01-17T18:36:46Z</dc:date>
    <item>
      <title>MPC8555CDS board does not boot 2.6 linux from BPS CD</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179866#M1285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;I have a MPC8555CDS board on which I run Linux 2.4 from a Freescale BPS iso image dated 2005.&lt;BR /&gt;However I need it to run Linux 2.6 and I downloaded the BPS iso CD image from this site (dated 17 October 2006, the latest I could find). The flash images provided on this CD do not work i.e. the linux 2.6.11 does not boot. I can boot the linux 2.4 with the filesystem of the 2006 CD but this means mixing different version of kernel and software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The linux 2.6 does not provide any text output. I can see some led's on the board flickering for 15 secs and that is it.&lt;BR /&gt;I am now trying nfs boot instead of ramboot or flashboot, but sofar no luck.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. I can build new kernels and rootsystems with ltib from the 2006 BSP CD, but no configuration builds a bootable linux.&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;BR /&gt;Some info:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;U-Boot 1.1.3 (FSL Development) (Oct 27 2006 - 10:43:18)&lt;BR /&gt;&lt;BR /&gt;CPU:&amp;nbsp;&amp;nbsp; 8555, Version: 1.1, (0x80790011)&lt;BR /&gt;Core:&amp;nbsp; E500, Version: 2.0, (0x80200020)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CPU: 499 MHz, CCB: 166 MHz,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR:&amp;nbsp; 83 MHz, LBC:&amp;nbsp; 41 MHz&lt;BR /&gt;L1:&amp;nbsp;&amp;nbsp;&amp;nbsp; D-cache 32 kB enabled&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I-cache 32 kB enabled&lt;BR /&gt;Board: CDS Version 0x11&lt;BR /&gt;CPU Board Revision 0.0 (0x0000)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PCI1: 32 bit, 33 MHz, sync&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PCI2: 32 bit, 66 MHz, async&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; Initializing&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SDRAM: 64 MB&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR: 256 MB&lt;BR /&gt;FLASH: 16 MB&lt;BR /&gt;L2 cache 256KB: enabled&lt;BR /&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="font-family: 'Courier New'; font-size: 10pt;"&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; TSEC0: PHY is Cicada Cis8204 (fc446)&lt;BR /&gt;TSEC1: PHY is Cicada Cis8204 (fc446)&lt;BR /&gt;TSEC0, TSEC1&lt;BR /&gt;The IP address of the board is currently set to 192.168.1.253&lt;BR /&gt;The MAC address is 00:E0:0C:00:00:FD&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv&lt;BR /&gt;&lt;SPAN style="font-family: 'Courier New'; font-size: 10pt;"&gt;ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;bootm $loadaddr $ramdiskaddr&lt;BR /&gt;nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;ff console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;bootm $loadaddr&lt;BR /&gt;bootdelay=10&lt;BR /&gt;baudrate=115200&lt;BR /&gt;loads_echo=1&lt;BR /&gt;ethaddr=00:E0:0C:00:00:FD&lt;BR /&gt;eth1addr=00:E0:0C:00:01:FD&lt;BR /&gt;eth2addr=00:E0:0C:00:02:FD&lt;BR /&gt;rootpath=/nfsroot&lt;BR /&gt;hostname=unknown&lt;BR /&gt;loadaddr=1000000&lt;BR /&gt;netdev=eth0&lt;BR /&gt;consoledev=ttyS1&lt;BR /&gt;ramdiskaddr=2000000&lt;BR /&gt;ethact=TSEC0&lt;BR /&gt;filesize=1416d6&lt;BR /&gt;fileaddr=1000000&lt;BR /&gt;gatewayip=192.168.1.1&lt;BR /&gt;netmask=255.255.255.0&lt;BR /&gt;ipaddr=192.168.1.253&lt;BR /&gt;serverip=192.168.1.1&lt;BR /&gt;flashrootfs=tftp $ramdiskaddr $ramdiskfile;prot off all;erase ffa00000 ffefffff;cp.b $ramdiskaddr ffa00000 3fffff;prot on all&lt;BR /&gt;flashlinux=tftp $loadaddr $bootfile;prot off all;erase ff800000 ff9fffff;cp.b $loadaddr ff800000 1fffff;prot on all&lt;BR /&gt;bootargs=root=/dev/ram rw ramdisk_size=10464 console=ttyS1,115200&lt;BR /&gt;othbootargs=ramdisk_size=10464&lt;BR /&gt;bootfile=/media/sda1/images/uImage&lt;BR /&gt;ramdiskfile=/media/sda1/images/rootfs.ext2.gz.uboot&lt;BR /&gt;bootcmd=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;bootm $loadaddr $ramdiskaddr&lt;BR /&gt;flashboot=setenv bootargs root=/dev/ram rw console=ttyS1,115200 ramdisk_size=10464;bootm ff800000 ffa00000&lt;BR /&gt;stdin=serial&lt;BR /&gt;stdout=serial&lt;BR /&gt;stderr=serial&lt;BR /&gt;&lt;BR /&gt;Environment size: 1483/8188 bytes&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Message Edited by robthales on &lt;SPAN class="date_text"&gt;2008-01-16&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;07:35 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2008 15:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179866#M1285</guid>
      <dc:creator>robthales</dc:creator>
      <dc:date>2008-01-16T15:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8555CDS board does not boot 2.6 linux from BPS CD</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179867#M1286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you have an early version of the CDS board that the new BSP isn't tuned for? I believe this BSP was targeted for CDC Ver. 1.1, Carrier Card Ver1.3 and Arcadia X3.1.&lt;BR /&gt;&lt;BR /&gt;Attached is the user's manual for the BSP. Have you verified that your dip switches correspond to the manual?&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;... Paul&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/MCUCOMM/965_um_mpc8555cds_k26_20061017.pdf" rel="nofollow" target="_self"&gt;UM_MPC8555CDS_K26_20061017.pdf&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-10-29&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;09:32 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2008 22:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179867#M1286</guid>
      <dc:creator>genuap</dc:creator>
      <dc:date>2008-01-16T22:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8555CDS board does not boot 2.6 linux from BPS CD</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179868#M1287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Paul,&lt;BR /&gt;&lt;BR /&gt;Thanks for the answer.&lt;BR /&gt;I believe you are right about versions. I tried the oldest BSP that contains linux 2.6, which is&amp;nbsp; 20050408. The linux from this iso image boots OK!&lt;BR /&gt;So I use an 'old' linux and the uboot and rootfs of the latest BSP.&lt;BR /&gt;&lt;BR /&gt;Rob&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2008 18:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179868#M1287</guid>
      <dc:creator>robthales</dc:creator>
      <dc:date>2008-01-17T18:36:46Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8555CDS board does not boot 2.6 linux from BPS CD</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179869#M1288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Another question struck me:&lt;BR /&gt;&lt;BR /&gt;Because I cannot build linux with the 20050408 BSP version but I can with the 20061017:&lt;BR /&gt;&lt;BR /&gt;How can I get this latest linux to work on my apparently older board?&lt;BR /&gt;What are the differences between CDS 1.0 and 1.1 (from a linux viewpoint)?&lt;BR /&gt;&lt;BR /&gt;Rob&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2008 18:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8555CDS-board-does-not-boot-2-6-linux-from-BPS-CD/m-p/179869#M1288</guid>
      <dc:creator>robthales</dc:creator>
      <dc:date>2008-01-17T18:54:15Z</dc:date>
    </item>
  </channel>
</rss>