<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: sd host controller driver for reading a linux image on a mx31 PDK board in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/sd-host-controller-driver-for-reading-a-linux-image-on-a-mx31/m-p/179862#M1284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to have MX31 silicon version TO2.0.1 in order to boot from SD/MMC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is Redboot support for booting from SD/MMC on MX31 (TO2.0.1) on Redboot 200841 and later versions. There is also a pre-built image that can boot from from SD (mx31_3stack_redboot_mmc.bin).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can use ATK to flash this image into SD card.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2009 21:30:58 GMT</pubDate>
    <dc:creator>fabio_estevam</dc:creator>
    <dc:date>2009-05-12T21:30:58Z</dc:date>
    <item>
      <title>sd host controller driver for reading a linux image on a mx31 PDK board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/sd-host-controller-driver-for-reading-a-linux-image-on-a-mx31/m-p/179861#M1283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I intend to boot linux off SD card on the mx31 3stack board. I hope this can be done by adding custom logic to U-boot/Redboot. But this would require a MMC/SD driver along with the host controller driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is&amp;nbsp; there a readymade driver in Uboot/Redboot to do this.&amp;nbsp; Would this minimal driver support reading linux uImage off the SD Card. If then how&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Joseph.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 May 2009 01:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/sd-host-controller-driver-for-reading-a-linux-image-on-a-mx31/m-p/179861#M1283</guid>
      <dc:creator>josephb</dc:creator>
      <dc:date>2009-05-10T01:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: sd host controller driver for reading a linux image on a mx31 PDK board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/sd-host-controller-driver-for-reading-a-linux-image-on-a-mx31/m-p/179862#M1284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You need to have MX31 silicon version TO2.0.1 in order to boot from SD/MMC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is Redboot support for booting from SD/MMC on MX31 (TO2.0.1) on Redboot 200841 and later versions. There is also a pre-built image that can boot from from SD (mx31_3stack_redboot_mmc.bin).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can use ATK to flash this image into SD card.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2009 21:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/sd-host-controller-driver-for-reading-a-linux-image-on-a-mx31/m-p/179862#M1284</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2009-05-12T21:30:58Z</dc:date>
    </item>
  </channel>
</rss>