<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: Problem in using MPC8260 in Master Mode</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-using-MPC8260-in-Master-Mode/m-p/179690#M1282</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you're not seeing CS0 move at all, then you've got trouble. Does it move at all? Even while HRSET is asserted?&lt;BR /&gt;&lt;BR /&gt;While HRESET is asserted it should toggle to retrieve the HR Reset Config Word. If this is not happening then the PLL's probably aren't locking.&lt;BR /&gt;&lt;BR /&gt;I would look into your clock - make sure it's stable.&lt;BR /&gt;&lt;BR /&gt;If it toggles during HRESET (to fetch the reset word) but not after reset is de-asserted, then I would make sure all of your TA signals (i.e. GTA) are pulled up. And also make sure you're loading the correct HW Config word into the processor.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Aug 2008 22:20:49 GMT</pubDate>
    <dc:creator>genuap</dc:creator>
    <dc:date>2008-08-14T22:20:49Z</dc:date>
    <item>
      <title>Problem in using MPC8260 in Master Mode</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-using-MPC8260-in-Master-Mode/m-p/179689#M1281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;I am using MPC8260 in master mode and the code is executed from flash at startup. The problem is that about 80% of the times the processor executes the code correctly and about 20% of the time it fails to execute the code. If the processor fails to boot from flash and PORESET or HRESET is asserted externally then it starts working again. A SRESET has no effect in this problem.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;When the startup is failed then the MPC even does not toggles RAM_CS of FLASH CS. It is completely dead. The power supply sequence is correct. ANy suggestions in this problem will be of great help to me.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Waiting for your reply,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Aug 2008 19:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-using-MPC8260-in-Master-Mode/m-p/179689#M1281</guid>
      <dc:creator>h_humble2001</dc:creator>
      <dc:date>2008-08-13T19:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in using MPC8260 in Master Mode</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-using-MPC8260-in-Master-Mode/m-p/179690#M1282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you're not seeing CS0 move at all, then you've got trouble. Does it move at all? Even while HRSET is asserted?&lt;BR /&gt;&lt;BR /&gt;While HRESET is asserted it should toggle to retrieve the HR Reset Config Word. If this is not happening then the PLL's probably aren't locking.&lt;BR /&gt;&lt;BR /&gt;I would look into your clock - make sure it's stable.&lt;BR /&gt;&lt;BR /&gt;If it toggles during HRESET (to fetch the reset word) but not after reset is de-asserted, then I would make sure all of your TA signals (i.e. GTA) are pulled up. And also make sure you're loading the correct HW Config word into the processor.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Aug 2008 22:20:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-in-using-MPC8260-in-Master-Mode/m-p/179690#M1282</guid>
      <dc:creator>genuap</dc:creator>
      <dc:date>2008-08-14T22:20:49Z</dc:date>
    </item>
  </channel>
</rss>