<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 16 Channel Adjustable Constant Current LED Driver</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/16-Channel-Adjustable-Constant-Current-LED-Driver/m-p/1385043#M12773</link>
    <description>&lt;P&gt;I'm looking for a drop in replacement for the TI&amp;nbsp;TLC5926IPWPR LED driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It's 16 channel constant current LED driver. Max current is set via an external resistor, but we can also adjust the current via the SPI interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does NXP have this as well? I do not need error detection feature. Just need to adjust the current via SPI bus.&lt;BR /&gt;&lt;BR /&gt;5mA to 61mA output current.&lt;/P&gt;</description>
    <pubDate>Fri, 10 Dec 2021 19:46:07 GMT</pubDate>
    <dc:creator>guitardenver</dc:creator>
    <dc:date>2021-12-10T19:46:07Z</dc:date>
    <item>
      <title>16 Channel Adjustable Constant Current LED Driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/16-Channel-Adjustable-Constant-Current-LED-Driver/m-p/1385043#M12773</link>
      <description>&lt;P&gt;I'm looking for a drop in replacement for the TI&amp;nbsp;TLC5926IPWPR LED driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It's 16 channel constant current LED driver. Max current is set via an external resistor, but we can also adjust the current via the SPI interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does NXP have this as well? I do not need error detection feature. Just need to adjust the current via SPI bus.&lt;BR /&gt;&lt;BR /&gt;5mA to 61mA output current.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Dec 2021 19:46:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/16-Channel-Adjustable-Constant-Current-LED-Driver/m-p/1385043#M12773</guid>
      <dc:creator>guitardenver</dc:creator>
      <dc:date>2021-12-10T19:46:07Z</dc:date>
    </item>
    <item>
      <title>Re: 16 Channel Adjustable Constant Current LED Driver</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/16-Channel-Adjustable-Constant-Current-LED-Driver/m-p/1385490#M12779</link>
      <description>&lt;P&gt;Hello Matt,&lt;/P&gt;
&lt;P&gt;There is not a drop in replacement for the TI TLC5926IPWPR currently available in our portfolio.&lt;/P&gt;
&lt;P&gt;The closest device is the PCA9745B: 16-channel SPI serial bus 57 mA/20 V constant current LED driver:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/PCA9745B.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;There is a table with all NXP’s LED controllers available in the following document, page 3:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/brochure/LED-CONTROLLERS-FINAL-DELIVERABLES.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 13 Dec 2021 08:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/16-Channel-Adjustable-Constant-Current-LED-Driver/m-p/1385490#M12779</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-12-13T08:43:48Z</dc:date>
    </item>
  </channel>
</rss>