<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: SC16IS762</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS762/m-p/1368878#M12510</link>
    <description>&lt;P&gt;VDD=2.5V support to Max 48MHz.&lt;/P&gt;
&lt;P&gt;VDD=3.3V support to Max 80MHz&lt;/P&gt;</description>
    <pubDate>Wed, 10 Nov 2021 03:01:16 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2021-11-10T03:01:16Z</dc:date>
    <item>
      <title>SC16IS762</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS762/m-p/1368812#M12509</link>
      <description>&lt;P&gt;&lt;STRONG&gt;What is the max frequency for the XTAL input of SC16IS762?&amp;nbsp; The datasheet only shows the max baud rate for the serial interface up to 5Mbps.&amp;nbsp; Per the formula for the baud rate, can I assume the max freq for the XTAL input is 60MHz?&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 00:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS762/m-p/1368812#M12509</guid>
      <dc:creator>qdinh</dc:creator>
      <dc:date>2021-11-10T00:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS762</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS762/m-p/1368878#M12510</link>
      <description>&lt;P&gt;VDD=2.5V support to Max 48MHz.&lt;/P&gt;
&lt;P&gt;VDD=3.3V support to Max 80MHz&lt;/P&gt;</description>
      <pubDate>Wed, 10 Nov 2021 03:01:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS762/m-p/1368878#M12510</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-11-10T03:01:16Z</dc:date>
    </item>
  </channel>
</rss>