<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364472#M12465</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you so much for quick response however the scripts you mentioned are for the new CLRC663 product family range.&lt;/P&gt;&lt;P&gt;Do you have something similar for the older version of these ICs namely the SLRc400 and CLRC632?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luke&lt;/P&gt;</description>
    <pubDate>Mon, 01 Nov 2021 09:36:27 GMT</pubDate>
    <dc:creator>software_memo</dc:creator>
    <dc:date>2021-11-01T09:36:27Z</dc:date>
    <item>
      <title>CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364416#M12462</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can anyone please provide some guidance for settings up the registers in either the CLRC632 or SLRC400 to send an inventory command to ISO15693 compliant cards? Any application notes or example code would be very much appreciated.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luke&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 08:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364416#M12462</guid>
      <dc:creator>software_memo</dc:creator>
      <dc:date>2021-11-01T08:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364468#M12464</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189748"&gt;@software_memo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is a script file available for this purpose, please kindly refer to&amp;nbsp;&lt;A href="https://www.nxp.com/downloads/en/software/210910.zip" target="_blank"&gt;https://www.nxp.com/downloads/en/software/210910.zip&lt;/A&gt;&amp;nbsp;for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 09:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364468#M12464</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-11-01T09:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364472#M12465</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you so much for quick response however the scripts you mentioned are for the new CLRC663 product family range.&lt;/P&gt;&lt;P&gt;Do you have something similar for the older version of these ICs namely the SLRc400 and CLRC632?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luke&lt;/P&gt;</description>
      <pubDate>Mon, 01 Nov 2021 09:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364472#M12465</guid>
      <dc:creator>software_memo</dc:creator>
      <dc:date>2021-11-01T09:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC632 or SLRC400 register settings and example code for ISO15693 inventory command</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364839#M12469</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189748"&gt;@software_memo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am sorry but no such kind of example available, we recommend CLRC663 plus for new design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 02 Nov 2021 06:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CLRC632-or-SLRC400-register-settings-and-example-code-for/m-p/1364839#M12469</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-11-02T06:00:43Z</dc:date>
    </item>
  </channel>
</rss>