<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCF2129 time errors in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1350667#M12247</link>
    <description>&lt;P&gt;I am using a PCF2129 RTC connected to a MC9S08QE16 via I2C. Normally, on power-up the correct time is shown on the MCU's display, but occasionally it displays a completely different time, which I then have to adjust using the application software. Also - I am employing the RTC's alarm function (only hours, minutes and seconds), and (again occasionally) the alarm triggers early although the alarm registers are correct. I have built 10 samples and only two units display this problem&lt;/P&gt;</description>
    <pubDate>Tue, 05 Oct 2021 13:58:19 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2021-10-05T13:58:19Z</dc:date>
    <item>
      <title>PCF2129 time errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1350667#M12247</link>
      <description>&lt;P&gt;I am using a PCF2129 RTC connected to a MC9S08QE16 via I2C. Normally, on power-up the correct time is shown on the MCU's display, but occasionally it displays a completely different time, which I then have to adjust using the application software. Also - I am employing the RTC's alarm function (only hours, minutes and seconds), and (again occasionally) the alarm triggers early although the alarm registers are correct. I have built 10 samples and only two units display this problem&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 13:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1350667#M12247</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2021-10-05T13:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2129 time errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1350821#M12249</link>
      <description>&lt;P&gt;Do you have a cross test with the good PCF2129 and issue board ?if no please try it!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Oct 2021 22:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1350821#M12249</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-10-05T22:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2129 time errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1353466#M12295</link>
      <description>&lt;P&gt;This is a bit problematic as the error only occurs every 3 or 4 days on an irregular basis. The las error occurred yesterday evening, after running for 5 days. This time I switched the unit on at 17:40 and the time was displayed as 00:40. I am currently running ten units, testing the time alarm function and power-down, wait, power-up cycling for two weeks - only two faults on one unit.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Oct 2021 10:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1353466#M12295</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2021-10-11T10:12:04Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2129 time errors</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1353576#M12298</link>
      <description>Please share with your schematic.</description>
      <pubDate>Mon, 11 Oct 2021 13:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129-time-errors/m-p/1353576#M12298</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-10-11T13:42:40Z</dc:date>
    </item>
  </channel>
</rss>