<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NVT2002DP(TSSOP) in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349477#M12221</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello. I recently purchased 30 NVT2002DP level shifters and left a message because I was curious about how to use them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm analyzing data sheets, and I wonder if pins 3 and 4 and 5 and 6 have differences in motion, or if we can simply use the same thing as having two signal paths.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To add explanation, I wonder if pin 3 (A1) and pin 4 (A2) can be used as independent level shift inputs/outputs, or if there is a dependent relationship between the two.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Oct 2021 08:23:07 GMT</pubDate>
    <dc:creator>songgoon</dc:creator>
    <dc:date>2021-10-01T08:23:07Z</dc:date>
    <item>
      <title>NVT2002DP(TSSOP)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349477#M12221</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello. I recently purchased 30 NVT2002DP level shifters and left a message because I was curious about how to use them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm analyzing data sheets, and I wonder if pins 3 and 4 and 5 and 6 have differences in motion, or if we can simply use the same thing as having two signal paths.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To add explanation, I wonder if pin 3 (A1) and pin 4 (A2) can be used as independent level shift inputs/outputs, or if there is a dependent relationship between the two.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 08:23:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349477#M12221</guid>
      <dc:creator>songgoon</dc:creator>
      <dc:date>2021-10-01T08:23:07Z</dc:date>
    </item>
    <item>
      <title>Re: NVT2002DP(TSSOP)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349544#M12223</link>
      <description>&lt;P&gt;Hello Songgoon,&lt;/P&gt;
&lt;P&gt;please refer to figure 1. in the &lt;A href="https://www.nxp.com/docs/en/data-sheet/NVT2001_NVT2002.pdf" target="_self"&gt;NVT2002&lt;/A&gt; datasheet. The A1 and A2 can be used independently. Only dependence is between the A1, A2, B1, B2 and the EN pin. If the pin is held low, the four pins are in high impedance state.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1633087314521.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158082i327D184A20FC27A4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1633087314521.png" alt="JozefKozon_0-1633087314521.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JozefKozon_0-1633087314521.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_1-1633087346556.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/158083i6E43282A84D69EF4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_1-1633087346556.png" alt="JozefKozon_1-1633087346556.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JozefKozon_1-1633087346556.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 11:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349544#M12223</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-10-01T11:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: NVT2002DP(TSSOP)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349548#M12224</link>
      <description>&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 11:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349548#M12224</guid>
      <dc:creator>songgoon</dc:creator>
      <dc:date>2021-10-01T11:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: NVT2002DP(TSSOP)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349553#M12225</link>
      <description>&lt;P&gt;Hello Songgoon,&lt;/P&gt;
&lt;P&gt;you welcome.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 01 Oct 2021 11:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NVT2002DP-TSSOP/m-p/1349553#M12225</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-10-01T11:47:26Z</dc:date>
    </item>
  </channel>
</rss>