<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: NXP UDA1334A Adafruit-I2Sdecoder for 24bit resolution</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-UDA1334A-Adafruit-I2Sdecoder-for-24bit-resolution/m-p/1343821#M12126</link>
    <description>&lt;P&gt;This IC had already EOL and no more related documentations supporting are available now.&lt;/P&gt;</description>
    <pubDate>Wed, 22 Sep 2021 08:09:22 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2021-09-22T08:09:22Z</dc:date>
    <item>
      <title>NXP UDA1334A Adafruit-I2Sdecoder for 24bit resolution</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-UDA1334A-Adafruit-I2Sdecoder-for-24bit-resolution/m-p/1341689#M12090</link>
      <description>&lt;P&gt;I am interfacing the Adafruit board for NXP-UDA1334A to a Bluetooth audio module, I can hear the clear audio output for 16bit resolution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to configure the module for 24 bit resolution, I get noisy output. My Bluetooth module is master and I am using left-justified, nobit delay, I2S output from master.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have correctly selected the SF0-SF1 lines both high.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to use re-sample frequency at master configuration as 44100 and 48000, but both gives same noise level.&lt;/P&gt;&lt;P&gt;I tried to use De-Emph to High but this also does not help much.&lt;/P&gt;&lt;P&gt;Is there any other setting I need to use for 24 bit operation?&lt;/P&gt;&lt;P&gt;I am only interfacing, BCLK, WSEL and DIN pins from adafruit board, the PLL pin grounded memaning hte chip is in audio mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Sep 2021 15:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-UDA1334A-Adafruit-I2Sdecoder-for-24bit-resolution/m-p/1341689#M12090</guid>
      <dc:creator>SujataLMtech</dc:creator>
      <dc:date>2021-09-16T15:36:14Z</dc:date>
    </item>
    <item>
      <title>Re: NXP UDA1334A Adafruit-I2Sdecoder for 24bit resolution</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-UDA1334A-Adafruit-I2Sdecoder-for-24bit-resolution/m-p/1343821#M12126</link>
      <description>&lt;P&gt;This IC had already EOL and no more related documentations supporting are available now.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 08:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-UDA1334A-Adafruit-I2Sdecoder-for-24bit-resolution/m-p/1343821#M12126</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-09-22T08:09:22Z</dc:date>
    </item>
  </channel>
</rss>