<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCA9703 current limit in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9703-current-limit/m-p/1342919#M12111</link>
    <description>&lt;P&gt;I am trying to drive a series of 35 SSRs with a quantity of shift registers&amp;nbsp; using a common SPI bus. The SSRs will draw 3mA each. My idea was to sink each 3 mA current through a different unique GPI pin when I command it low, as a low-side switch . so one GPI pin is for only one SSR. Can I do this with the PCA9703? It seems that I can't, and the device cannot tolerate such current. Which is it?&lt;/P&gt;</description>
    <pubDate>Mon, 20 Sep 2021 20:07:55 GMT</pubDate>
    <dc:creator>gmarq922</dc:creator>
    <dc:date>2021-09-20T20:07:55Z</dc:date>
    <item>
      <title>PCA9703 current limit</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9703-current-limit/m-p/1342919#M12111</link>
      <description>&lt;P&gt;I am trying to drive a series of 35 SSRs with a quantity of shift registers&amp;nbsp; using a common SPI bus. The SSRs will draw 3mA each. My idea was to sink each 3 mA current through a different unique GPI pin when I command it low, as a low-side switch . so one GPI pin is for only one SSR. Can I do this with the PCA9703? It seems that I can't, and the device cannot tolerate such current. Which is it?&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 20:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9703-current-limit/m-p/1342919#M12111</guid>
      <dc:creator>gmarq922</dc:creator>
      <dc:date>2021-09-20T20:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9703 current limit</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9703-current-limit/m-p/1343819#M12125</link>
      <description>&lt;P&gt;Each input pin of PCA9703 can sink 100uA.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Sep 2021 08:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9703-current-limit/m-p/1343819#M12125</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-09-22T08:07:01Z</dc:date>
    </item>
  </channel>
</rss>