<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックMAC57D5MB Canbus cannot receive messages from Arduino</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MAC57D5MB-Canbus-cannot-receive-messages-from-Arduino/m-p/1342580#M12104</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have problems with receiving messages from Arduino(with seeed canbus transceiver/controller) as MAC57D5MB as a transmitter. details below:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I can send from MAC57D5MB to arduino with no problem and accurate data being received. However, they have different bit rates of 500kbps(arduino) and 250kbps(MAC57D5MB).&lt;/LI&gt;&lt;LI&gt;both transceiver have 120 ohms resistors&lt;/LI&gt;&lt;LI&gt;MAC57D5MB uses library of MQX4.2 Libraries and arduino uses mcp_can libraries.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I tried manipulating the codes from MAC57D5MB by enabling/disabling the FIFO and Message Buffer but no progress.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I also tried manipulating the bit rate from both controllers from 125kbps to 1mbps by different combinations but no progress.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I am sure that I have inputted the correct CAN IDENTIFIER for both controllers.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I suspect that the CAN ID is not being recognized by the MAC57D5MB. Please confirm if my idea is correct.&lt;/P&gt;&lt;P&gt;attached are source codes. hope to hear from you guys soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;</description>
    <pubDate>Mon, 20 Sep 2021 03:45:35 GMT</pubDate>
    <dc:creator>johnkevintoral</dc:creator>
    <dc:date>2021-09-20T03:45:35Z</dc:date>
    <item>
      <title>MAC57D5MB Canbus cannot receive messages from Arduino</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MAC57D5MB-Canbus-cannot-receive-messages-from-Arduino/m-p/1342580#M12104</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have problems with receiving messages from Arduino(with seeed canbus transceiver/controller) as MAC57D5MB as a transmitter. details below:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;I can send from MAC57D5MB to arduino with no problem and accurate data being received. However, they have different bit rates of 500kbps(arduino) and 250kbps(MAC57D5MB).&lt;/LI&gt;&lt;LI&gt;both transceiver have 120 ohms resistors&lt;/LI&gt;&lt;LI&gt;MAC57D5MB uses library of MQX4.2 Libraries and arduino uses mcp_can libraries.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I tried manipulating the codes from MAC57D5MB by enabling/disabling the FIFO and Message Buffer but no progress.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I also tried manipulating the bit rate from both controllers from 125kbps to 1mbps by different combinations but no progress.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;I am sure that I have inputted the correct CAN IDENTIFIER for both controllers.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I suspect that the CAN ID is not being recognized by the MAC57D5MB. Please confirm if my idea is correct.&lt;/P&gt;&lt;P&gt;attached are source codes. hope to hear from you guys soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;</description>
      <pubDate>Mon, 20 Sep 2021 03:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MAC57D5MB-Canbus-cannot-receive-messages-from-Arduino/m-p/1342580#M12104</guid>
      <dc:creator>johnkevintoral</dc:creator>
      <dc:date>2021-09-20T03:45:35Z</dc:date>
    </item>
  </channel>
</rss>