<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCF2127 communication problem in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-communication-problem/m-p/1339885#M12074</link>
    <description>&lt;P&gt;We are using PCF2127. Several PCBs have the same problem. During communication over I2C the IC reports a NAK after some write request. This happens after a several read / write operations but every time at the same point.&lt;/P&gt;&lt;P&gt;IC has this issue only at the first start. When I disconnect the battery from the IC and plug it back in (do a full reset), the device works fine until the next power cycle.&lt;/P&gt;&lt;P&gt;Can I reset the IC over I2C command without disconnecting the battery?&lt;/P&gt;</description>
    <pubDate>Wed, 15 Sep 2021 06:50:20 GMT</pubDate>
    <dc:creator>Konstantin_ch</dc:creator>
    <dc:date>2021-09-15T06:50:20Z</dc:date>
    <item>
      <title>PCF2127 communication problem</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-communication-problem/m-p/1339885#M12074</link>
      <description>&lt;P&gt;We are using PCF2127. Several PCBs have the same problem. During communication over I2C the IC reports a NAK after some write request. This happens after a several read / write operations but every time at the same point.&lt;/P&gt;&lt;P&gt;IC has this issue only at the first start. When I disconnect the battery from the IC and plug it back in (do a full reset), the device works fine until the next power cycle.&lt;/P&gt;&lt;P&gt;Can I reset the IC over I2C command without disconnecting the battery?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Sep 2021 06:50:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-communication-problem/m-p/1339885#M12074</guid>
      <dc:creator>Konstantin_ch</dc:creator>
      <dc:date>2021-09-15T06:50:20Z</dc:date>
    </item>
  </channel>
</rss>