<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックUsing PCA9548A with upstream slave (after configuration)</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Using-PCA9548A-with-upstream-slave-after-configuration/m-p/1334303#M11984</link>
    <description>&lt;P&gt;We are trying to use the PCA9548A with a downstream master device.&amp;nbsp; Is it possible to use the upstream master to configure the Control Block to connect to the downstream master, then after this configuration, reconfigure the upstream device to be a slave such that the downstream master can write data to the upstream slave?&amp;nbsp; Based on the PCA9548A block diagram and app note, the PCA9548A operates like a wire after configuration with clock/data able to go in either direction.&amp;nbsp; Do you see any issues with this plan?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, Ted&lt;/P&gt;</description>
    <pubDate>Thu, 02 Sep 2021 18:53:20 GMT</pubDate>
    <dc:creator>twolfe</dc:creator>
    <dc:date>2021-09-02T18:53:20Z</dc:date>
    <item>
      <title>Using PCA9548A with upstream slave (after configuration)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Using-PCA9548A-with-upstream-slave-after-configuration/m-p/1334303#M11984</link>
      <description>&lt;P&gt;We are trying to use the PCA9548A with a downstream master device.&amp;nbsp; Is it possible to use the upstream master to configure the Control Block to connect to the downstream master, then after this configuration, reconfigure the upstream device to be a slave such that the downstream master can write data to the upstream slave?&amp;nbsp; Based on the PCA9548A block diagram and app note, the PCA9548A operates like a wire after configuration with clock/data able to go in either direction.&amp;nbsp; Do you see any issues with this plan?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, Ted&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 18:53:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Using-PCA9548A-with-upstream-slave-after-configuration/m-p/1334303#M11984</guid>
      <dc:creator>twolfe</dc:creator>
      <dc:date>2021-09-02T18:53:20Z</dc:date>
    </item>
    <item>
      <title>Re: Using PCA9548A with upstream slave (after configuration)</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Using-PCA9548A-with-upstream-slave-after-configuration/m-p/1335758#M12012</link>
      <description>&lt;P&gt;Could you please give us your application simple diagram?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 03:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Using-PCA9548A-with-upstream-slave-after-configuration/m-p/1335758#M12012</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-09-07T03:17:25Z</dc:date>
    </item>
  </channel>
</rss>