<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Select  ISO1443A  operation with CLRC663</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1332016#M11945</link>
    <description>&lt;P&gt;Hi Fabian,&lt;/P&gt;&lt;P&gt;Thank you for following this up. I have again tried to get the software going.&lt;/P&gt;&lt;P&gt;I have relooked at the SPI communications, as originally I had an issue there, and I am happy that this is working correctly.&lt;/P&gt;&lt;P&gt;I’m able to receive the REQA response from the card and I have tried this with multiple DESFire and Mifare classic cards. The issue still arises when I try to get the “Answer to Select” from the cards to perform the anti-collision sequence. All the cards do not respond with anything and I time out waiting for an answer.&amp;nbsp; I removed the timeout and just looked for a response, this still didn’t work so it isn’t a lag issue.&lt;/P&gt;&lt;P&gt;I have tried to test the signal by putting a CRO on the test points (TP1 and TP2) on the CLEV6630ARD board. This puts a drain on the antenna and the cards no longer respond to the REQA. I thought that maybe the power was an issue and I have applied a beefed up power supply.&amp;nbsp; This made no difference.&lt;/P&gt;&lt;P&gt;I feel that the antenna might not be providing enough power for the cards to respond with anything more than the answer to REQA.&lt;/P&gt;&lt;P&gt;After being though this for so long and I feel that I now know much more about the chip I’m surprised that I am having issues getting the simple communications interface going.&amp;nbsp; I was expecting that following the sample codes would just work.&amp;nbsp; I’m now wondering if I have an issue with the board (hardware).&amp;nbsp; I think that this is unlikely but given the trouble that I am having I can’t rule this out. I’m a little disheartened with getting this going, since it only took me 3 hours to get the PN532 working.&lt;/P&gt;&lt;P&gt;If you have any other ideas I would love to hear them, as I think that I have tried everything.&lt;/P&gt;&lt;P&gt;The only question that I have; is the CLEV6630ARD board designed to have full communications with the cards or just able to detect the card’s presence?&lt;/P&gt;</description>
    <pubDate>Tue, 31 Aug 2021 00:08:45 GMT</pubDate>
    <dc:creator>Anjary</dc:creator>
    <dc:date>2021-08-31T00:08:45Z</dc:date>
    <item>
      <title>Select  ISO1443A  operation with CLRC663</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1327366#M11867</link>
      <description>&lt;P&gt;I have an issue with the Select card using the CLRC663.&lt;/P&gt;&lt;P&gt;I'm communicating with the chip via the SPI interface without using the NXP library. I'm currently able to get the ATQA response from the REQA command. But as soon as I attempt sending the select card for anti-collision I get no response from the card.&amp;nbsp; At least this is what the CLRC663 chip is telling me.&lt;/P&gt;&lt;P&gt;I have tried multiple things and checked all the register setting them to values that I believe should work.&lt;/P&gt;&lt;P&gt;The process that I am currently trying is using the following sequence for setting the registers:&lt;/P&gt;&lt;P&gt;Set_Timer_Control(TIMER_0_SELECTED, CLRC663_TCONTROL_STOPRX | CLRC663_TCONTROL_START_TX_END | CLRC663_TCONTROL_AUTO_RESTART | CLRC663_TCONTROL_CLK_13MHZ); // configure Timer 0. Set timer to 13.56 MHz clock, start at the end of Tx, Auto restart and stop after Rx.&lt;BR /&gt;Set_Timer_Control(TIMER_1_SELECTED, CLRC663_TCONTROL_STOPRX | CLRC663_TCONTROL_START_TX_END | CLRC633_TCONTROL_1_CASCADE | CLRC663_TCONTROL_CLK_13MHZ); // configure Timer 1. Set timer to 13.56 MHz clock, start at the end of Timer 0, Auto restart and stop after Rx.&lt;BR /&gt;Set_Timer_Control(TIMER_2_SELECTED, CLRC663_TCONTROL_2_LFO_TRIMMING_NO_UNDERFLOW | CLRC663_TCONTROL_CLK_13MHZ); // configure Timer 2. Set timer to 13.56 MHz clock. Used for LFO trimming.&lt;BR /&gt;Set_Timer_Reload(TIMER_2_SELECTED, 0x03FF);&lt;BR /&gt;Set_Timer_Control(TIMER_3_SELECTED, TCONTROL_CLK_13MHZ); // configure Timer 3. Not started, set to 13.56 MHz clock.&lt;BR /&gt;WriteRegisterByte(FIFO_CONTROL, 0xB0);&amp;nbsp; // Flush FIFO&lt;BR /&gt;WriteRegisterByte(RX_BIT_CTRL, 0x80); // Receive bits after collision replaced with zeros.&lt;BR /&gt;WriteRegisterByte(DRV_MODE, CLRC663_DRVMODE_TX2INV); // Invert transmitter 2 at pin&lt;BR /&gt;WriteRegisterByte(TX_AMP, 0x00); // Output Amplitude 0; TVDD 100mV&lt;BR /&gt;WriteRegisterByte(DRV_CON, 0x01); // Tx Envelope&lt;BR /&gt;// WriteRegisterByte(TXL, 0x05); // Factory set. Don't change?&lt;BR /&gt;WriteRegisterByte(RX_SOF_DETECTION, 0x00); // Clear SOF detection&lt;BR /&gt;WriteRegisterByte(RECEIVE, 0x12); // Signal over envelope (ISO14443A) collision detection 1/2 signal strength.&lt;BR /&gt;// Load Protocol&lt;BR /&gt;WriteRegisterByte(COMMAND, 0x00)&amp;nbsp; // Command Idle.&lt;BR /&gt;WriteRegisterByte(FIFO_CONTROL, 0xB0);&amp;nbsp; // Flush FIFO&lt;/P&gt;&lt;P&gt;WriteRegisterByte(IRQ0, 0x7F); // Clear the interrupts&lt;BR /&gt;WriteRegisterByte(IRQ1, 0x7F);&lt;BR /&gt;WriteRegisterByte(FIFO_DATA, 0x00); // Load protocol for ISO-14443A&lt;BR /&gt;WriteRegisterByte(FIFO_DATA, 0x00);&lt;BR /&gt;WriteRegisterByte(COMMAND, COMMAND_LOAD_PROTOCOL);&lt;BR /&gt;WriteRegisterByte(IRQ0_EN, IRQ0_ENABLE_IDLE_IRQ); // Enable IRQ sources: Idle&lt;BR /&gt;while ( !(Get_IRQ0_Value() &amp;amp; IRQ0_IDLE_IRQ) ) // Wait for Idle. Command to finish.&lt;BR /&gt;;&lt;BR /&gt;WriteRegisterByte(FIFO_CTRL, 0xB0);&lt;BR /&gt;// Apply Register Set.&lt;BR /&gt;WriteRegisterByte(TX_CRC_PRESET, 0x18); // Preset value 0x6363, CRC16 - CRC not used.&lt;BR /&gt;WriteRegisterByte(RX_CRC_PRESET, 0x18); // Preset value 0x6363, CRC16 - CRC not used.&lt;BR /&gt;WriteRegisterByte(TX_DATA_NUM, 0x08); // Data is sent!&lt;BR /&gt;WriteRegisterByte(TX_MODE_WIDTH, 0x20); // Length of pulse modulation in Carrier&lt;BR /&gt;WriteRegisterByte(TX_SYM_1_0_BURST_LEN, 0x00); // Symbol 0 and 1 burst lengths are 8 bits.&lt;BR /&gt;WriteRegisterByte(FRAME_CTRL, 0xCF); // Start symbol = Symbol 2; Stop symbol = Symbol 2.&lt;BR /&gt;WriteRegisterByte(RX_CTRL, 0x04); // Rx Baudrate 106k baud&lt;BR /&gt;WriteRegisterByte(RX_THRESHOLD, 0x32); // Set minimum levels for Rx and phase shift.&lt;BR /&gt;WriteRegisterByte(RX_ANALOG, 0x00); // Set gain and filter levels.&lt;BR /&gt;WriteRegisterByte(RX_WAIT, 0x90); // Set Rx waiting time.&lt;BR /&gt;WriteRegisterByte(TX_WAIT_CTRL, 0xC0); // Wait until the end of the Rx data.&lt;BR /&gt;WriteRegisterByte(TX_WAIT_LO, 0x0B); // Wait time between the receive and send data streams.&lt;BR /&gt;Set_Timer_Reload(TIMER_0_SELECTED, 0x08DB);&lt;BR /&gt;Set_Timer_Reload(TIMER_1_SELECTED, 0x0000);&lt;BR /&gt;WriteRegisterByte(DRV_MODE, 0X89);&lt;/P&gt;&lt;P&gt;WriteRegisterByte(STATUS, 0x00); // Mifare Crypto1 is disabled.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The selection consists of:&lt;/P&gt;&lt;P&gt;WriteRegisterByte(TX_DATA_NUM, 0x08); // Data is sent!&lt;BR /&gt;WriteRegisterByte(RX_BIT_CTRL, 0x00); // Cleared to look for a collision.&lt;BR /&gt;WriteRegisterByte(COMMAND, 0x00)&amp;nbsp; // Command Idle.&lt;/P&gt;&lt;P&gt;WriteRegisterByte(FIFO_CONTROL, 0xB0);&amp;nbsp; // Flush FIFO&lt;/P&gt;&lt;P&gt;WriteRegisterByte(TX_DATA_NUM, 0x0F); // Data is sent!&lt;BR /&gt;WriteRegisterByte(IRQ0_EN, IRQ0_ENABLE_RX_IRQ | IRQ0_ENABLE_ERR_IRQ); // Enable IRQ sources: Idle&lt;BR /&gt;WriteRegisterByte(FIFO_DATA, 0x93); // Write Select Command into FIFO&lt;BR /&gt;WriteRegisterByte(FIFO_DATA, 0x20);&lt;BR /&gt;WriteRegisterByte(COMMAND, COMMAND_TRANSCEIVE);&lt;/P&gt;&lt;P&gt;IRQ0_Value = Get_IRQ0_Value();&lt;BR /&gt;IRQ1_Value = Get_IRQ1_Value();&lt;BR /&gt;while ( !(IRQ1_Value &amp;amp; IRQ1_TIMER_1) ) // While the timer interrupt hasn't triggered.&lt;BR /&gt;{&lt;BR /&gt;IRQ1_Value = Get_IRQ1_Value();&lt;BR /&gt;if (IRQ0_Value &amp;amp; IRQ0_RX_IRQ)&lt;BR /&gt;break;&lt;BR /&gt;IRQ0_Value = Get_IRQ0_Value();&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;WriteRegisterByte(COMMAND, 0x00)&amp;nbsp; // Command Idle.&lt;/P&gt;&lt;P&gt;FifoDataLength = ReadRegisterByte(FIFO_LENGTH);&lt;BR /&gt;ReadRegisterArray(FIFO_DATA, ResponseDataArray, FifoDataLength);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The timers are set up so that a time out will occur if the card does not respond, which would be the case if a card is not present.&lt;/P&gt;&lt;P&gt;When I run the same sequence but have the REQA as the data being sent then the card responds.&lt;/P&gt;&lt;P&gt;What I'm not sure is if the registry settings are correct. Also I assume that all the data that is in the FIFO is sent during the Transceive command&amp;nbsp; writing (0x00, 0x07) and not just the first byte.&amp;nbsp; I haven't found any where to set the number of bytes to be sent and it appears that it is all the data in the FIFO (fifo length).&lt;/P&gt;&lt;P&gt;I have tried to send the REQA first and then the Select card after getting a response but this also fails to obtain a response from the card.&lt;/P&gt;&lt;P&gt;I have already been through the Application Note that covers the Card selection. I moved on from that as it didn't have any timing to check if the card was detected. This also failed to elicit a response from the card or at least the CLRC663 did not give an acknowledgement that the card had responded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another side question while I'm going I noticed that the clear FIFO command that is put in the sample codes is 0xB0, I don't understand why the LoAlert bit is being written to when the data sheet states that it is a read only bit? To me the value should be 0x90 for clearing the FIFO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Aug 2021 04:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1327366#M11867</guid>
      <dc:creator>Anjary</dc:creator>
      <dc:date>2021-08-23T04:34:57Z</dc:date>
    </item>
    <item>
      <title>Re: Select  ISO1443A  operation with CLRC663</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1328175#M11891</link>
      <description>&lt;P&gt;Just to follow up the document that I had originally used for the communication protocol is AN12657 (Using the RC663 without Library), this allowed me to get the REQA going, but the select for doing the collision detection doesn't appear to work. At least the card response is not detected.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 03:37:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1328175#M11891</guid>
      <dc:creator>Anjary</dc:creator>
      <dc:date>2021-08-24T03:37:12Z</dc:date>
    </item>
    <item>
      <title>Re: Select  ISO1443A  operation with CLRC663</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1328904#M11899</link>
      <description>&lt;P&gt;Hello Anjary.&lt;/P&gt;
&lt;P&gt;I hope you are doing great, please find the next link for an example that might help you with your implementation.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/how-to-communicate-between-LPC1769-and-RC663-via-SPI-based-on/ta-p/1303617" target="_blank"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/how-to-communicate-between-LPC1769-and-RC663-via-SPI-based-on/ta-p/1303617&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Aug 2021 21:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1328904#M11899</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2021-08-24T21:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: Select  ISO1443A  operation with CLRC663</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1329013#M11901</link>
      <description>&lt;P&gt;Hi Fabian,&lt;/P&gt;&lt;P&gt;Thanks for the link I will look into it and see what I can discover.&amp;nbsp; At a quick glance, looks similar to want I have already done but I have to have a better look.&lt;/P&gt;&lt;P&gt;&amp;nbsp; It might take me a day or two to look closely, as I have been pulled onto another task for the moment.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 02:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1329013#M11901</guid>
      <dc:creator>Anjary</dc:creator>
      <dc:date>2021-08-25T02:42:33Z</dc:date>
    </item>
    <item>
      <title>Re: Select  ISO1443A  operation with CLRC663</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1332016#M11945</link>
      <description>&lt;P&gt;Hi Fabian,&lt;/P&gt;&lt;P&gt;Thank you for following this up. I have again tried to get the software going.&lt;/P&gt;&lt;P&gt;I have relooked at the SPI communications, as originally I had an issue there, and I am happy that this is working correctly.&lt;/P&gt;&lt;P&gt;I’m able to receive the REQA response from the card and I have tried this with multiple DESFire and Mifare classic cards. The issue still arises when I try to get the “Answer to Select” from the cards to perform the anti-collision sequence. All the cards do not respond with anything and I time out waiting for an answer.&amp;nbsp; I removed the timeout and just looked for a response, this still didn’t work so it isn’t a lag issue.&lt;/P&gt;&lt;P&gt;I have tried to test the signal by putting a CRO on the test points (TP1 and TP2) on the CLEV6630ARD board. This puts a drain on the antenna and the cards no longer respond to the REQA. I thought that maybe the power was an issue and I have applied a beefed up power supply.&amp;nbsp; This made no difference.&lt;/P&gt;&lt;P&gt;I feel that the antenna might not be providing enough power for the cards to respond with anything more than the answer to REQA.&lt;/P&gt;&lt;P&gt;After being though this for so long and I feel that I now know much more about the chip I’m surprised that I am having issues getting the simple communications interface going.&amp;nbsp; I was expecting that following the sample codes would just work.&amp;nbsp; I’m now wondering if I have an issue with the board (hardware).&amp;nbsp; I think that this is unlikely but given the trouble that I am having I can’t rule this out. I’m a little disheartened with getting this going, since it only took me 3 hours to get the PN532 working.&lt;/P&gt;&lt;P&gt;If you have any other ideas I would love to hear them, as I think that I have tried everything.&lt;/P&gt;&lt;P&gt;The only question that I have; is the CLEV6630ARD board designed to have full communications with the cards or just able to detect the card’s presence?&lt;/P&gt;</description>
      <pubDate>Tue, 31 Aug 2021 00:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Select-ISO1443A-operation-with-CLRC663/m-p/1332016#M11945</guid>
      <dc:creator>Anjary</dc:creator>
      <dc:date>2021-08-31T00:08:45Z</dc:date>
    </item>
  </channel>
</rss>