<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCA9506 not acknowledge in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1324920#M11812</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I’m using the PCA9506 port expander. Power and ground are hooked up correctly. All address pins are pulled high - thus the 7bit address should be 0b0100111+R/!W. I am using a clock speed of 100kHz. I’ve scoped the signal and the first byte looks correct but there is no acknowledge from the chip and I can’t proceed from here. Am I missing something? Is my address incorrect? Or do I need to hold the !reset or !OE pins in a certain state during this frame? Thank you!&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Aug 2021 19:12:33 GMT</pubDate>
    <dc:creator>Benkg</dc:creator>
    <dc:date>2021-08-17T19:12:33Z</dc:date>
    <item>
      <title>PCA9506 not acknowledge</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1324920#M11812</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I’m using the PCA9506 port expander. Power and ground are hooked up correctly. All address pins are pulled high - thus the 7bit address should be 0b0100111+R/!W. I am using a clock speed of 100kHz. I’ve scoped the signal and the first byte looks correct but there is no acknowledge from the chip and I can’t proceed from here. Am I missing something? Is my address incorrect? Or do I need to hold the !reset or !OE pins in a certain state during this frame? Thank you!&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Aug 2021 19:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1324920#M11812</guid>
      <dc:creator>Benkg</dc:creator>
      <dc:date>2021-08-17T19:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9506 not acknowledge</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1325014#M11814</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Address is correct.&lt;/P&gt;
&lt;P&gt;PCA9506 is compatible with I2C-bus standard mode (100 kHz).&lt;/P&gt;
&lt;P&gt;!OE pin should be LOW for normal operation and !RESET pin should be HIGH for normal operation. Timing requirements for these pins can be found in Table 11 of the datasheet: &lt;A href="https://www.nxp.com/docs/en/data-sheet/PCA9505_9506.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/PCA9505_9506.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please performed a swap test (changing the ‘failing’ PCA9506 for a new device), just to make sure the problem is not the device itself.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jose&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 00:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1325014#M11814</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2021-08-18T00:23:23Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9506 not acknowledge</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1325128#M11816</link>
      <description>&lt;P&gt;Thank you, I don’t think I was driving the enable and reset pins correctly. I will try this and swap if it doesn’t work. Thanks Jose!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 03:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9506-not-acknowledge/m-p/1325128#M11816</guid>
      <dc:creator>Benkg</dc:creator>
      <dc:date>2021-08-18T03:31:43Z</dc:date>
    </item>
  </channel>
</rss>