<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPU initialization failed in u-boot-2018 with SMARC-FIMX6 quad board in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/GPU-initialization-failed-in-u-boot-2018-with-SMARC-FIMX6-quad/m-p/1323247#M11793</link>
    <description>&lt;P&gt;I am using SMARC-FIMX6 quad board and SMARC-FIMX6 solo board, and I am loading a firmware using USB, so in solo board the firmware is properly loading and the GPU initialization happened properly,&lt;/P&gt;&lt;P&gt;The same firmware when I run in Quad board, its failing in the GPU initialization, so please help me to resolve the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Here I attached the log, please verify&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Winston.&lt;/P&gt;</description>
    <pubDate>Fri, 13 Aug 2021 13:06:46 GMT</pubDate>
    <dc:creator>winstonjacob</dc:creator>
    <dc:date>2021-08-13T13:06:46Z</dc:date>
    <item>
      <title>GPU initialization failed in u-boot-2018 with SMARC-FIMX6 quad board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/GPU-initialization-failed-in-u-boot-2018-with-SMARC-FIMX6-quad/m-p/1323247#M11793</link>
      <description>&lt;P&gt;I am using SMARC-FIMX6 quad board and SMARC-FIMX6 solo board, and I am loading a firmware using USB, so in solo board the firmware is properly loading and the GPU initialization happened properly,&lt;/P&gt;&lt;P&gt;The same firmware when I run in Quad board, its failing in the GPU initialization, so please help me to resolve the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Here I attached the log, please verify&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Winston.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 13:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/GPU-initialization-failed-in-u-boot-2018-with-SMARC-FIMX6-quad/m-p/1323247#M11793</guid>
      <dc:creator>winstonjacob</dc:creator>
      <dc:date>2021-08-13T13:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: GPU initialization failed in u-boot-2018 with SMARC-FIMX6 quad board</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/GPU-initialization-failed-in-u-boot-2018-with-SMARC-FIMX6-quad/m-p/1323421#M11797</link>
      <description>&lt;P&gt;Hi Winston&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the same file can not be used for i.MX6Q and i.MX6S as they are different processors.&lt;/P&gt;
&lt;P&gt;For gpu issue one can check if gpu clocks are enabled in CCM Clock Gating Register 1 CCM_CCGR1,&lt;/P&gt;
&lt;P&gt;CCGR3.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Sat, 14 Aug 2021 00:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/GPU-initialization-failed-in-u-boot-2018-with-SMARC-FIMX6-quad/m-p/1323421#M11797</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-08-14T00:25:16Z</dc:date>
    </item>
  </channel>
</rss>