<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: netdb.h file for MPC8313ERDB</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/netdb-h-file-for-MPC8313ERDB/m-p/173954#M1177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Ak79,&lt;/P&gt;&lt;P&gt;On my Linux machine, the netdb.h file is under the same directory as all the other regular include files for compiling MPC8313E targeted linux apps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is where I found it on my machine:&lt;/P&gt;&lt;B&gt;&lt;/B&gt;&lt;P&gt;&lt;B&gt;alan@raptor:/opt/mtwk/usr/local/powerpc-linux/gcc-3.4.3-glibc-2.3.3/powerpc-linux/include$&lt;/B&gt;&lt;/P&gt;&lt;I&gt;ls net*.h&lt;/I&gt;&lt;B&gt;&lt;/B&gt;&lt;P&gt;&lt;B&gt;netdb.h&lt;/B&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also know that busybox uses netdb.h, so I'd assume it would be a standard install when LTIB is installed, but as I've recompiled busybox to add some options that were not in the default build of the MPC8313E Linux BSP, I guess there is a chance that the .h file is installed if you build busybox from the ./ltib --configure menu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;abartky&lt;/P&gt;&lt;FONT face="Arial" size="2"&gt;&lt;/FONT&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Dec 2007 05:35:05 GMT</pubDate>
    <dc:creator>abartky</dc:creator>
    <dc:date>2007-12-19T05:35:05Z</dc:date>
    <item>
      <title>netdb.h file for MPC8313ERDB</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/netdb-h-file-for-MPC8313ERDB/m-p/173953#M1176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; I have an application built on the PC which transmits data to a given IP. I am trying to port the same on to the MPC8313ERDB. I am unable to find the netdb.h file from the board source code. I am unable to perform some of the socket related functions. Is there a alternative/replacement for this netdb.h file??&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Ak79&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2007 04:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/netdb-h-file-for-MPC8313ERDB/m-p/173953#M1176</guid>
      <dc:creator>ak79</dc:creator>
      <dc:date>2007-12-19T04:13:53Z</dc:date>
    </item>
    <item>
      <title>Re: netdb.h file for MPC8313ERDB</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/netdb-h-file-for-MPC8313ERDB/m-p/173954#M1177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Ak79,&lt;/P&gt;&lt;P&gt;On my Linux machine, the netdb.h file is under the same directory as all the other regular include files for compiling MPC8313E targeted linux apps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is where I found it on my machine:&lt;/P&gt;&lt;B&gt;&lt;/B&gt;&lt;P&gt;&lt;B&gt;alan@raptor:/opt/mtwk/usr/local/powerpc-linux/gcc-3.4.3-glibc-2.3.3/powerpc-linux/include$&lt;/B&gt;&lt;/P&gt;&lt;I&gt;ls net*.h&lt;/I&gt;&lt;B&gt;&lt;/B&gt;&lt;P&gt;&lt;B&gt;netdb.h&lt;/B&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also know that busybox uses netdb.h, so I'd assume it would be a standard install when LTIB is installed, but as I've recompiled busybox to add some options that were not in the default build of the MPC8313E Linux BSP, I guess there is a chance that the .h file is installed if you build busybox from the ./ltib --configure menu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;abartky&lt;/P&gt;&lt;FONT face="Arial" size="2"&gt;&lt;/FONT&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2007 05:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/netdb-h-file-for-MPC8313ERDB/m-p/173954#M1177</guid>
      <dc:creator>abartky</dc:creator>
      <dc:date>2007-12-19T05:35:05Z</dc:date>
    </item>
  </channel>
</rss>