<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックMSDI Inputs as Outputs</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MSDI-Inputs-as-Outputs/m-p/1321332#M11762</link>
    <description>&lt;P&gt;This is regarding the Multi Switch Detector Interface ICs.&lt;/P&gt;&lt;P&gt;On the datasheets for the MC33972, MC33975, MC34972 and MC34975, it's shown how the input wetting current supplies can be used like outputs to drive a small load like an LED.&lt;/P&gt;&lt;P&gt;On the datasheets for the MC33978, MC34978, CD1020 and CD1030, this application is not mentioned, but at a first glance it seems that there is no reason why these ICs wouldn't be able to do this as well. Is someone able to confirm that this works on these ICs too?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Tue, 10 Aug 2021 21:09:52 GMT</pubDate>
    <dc:creator>mark512</dc:creator>
    <dc:date>2021-08-10T21:09:52Z</dc:date>
    <item>
      <title>MSDI Inputs as Outputs</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MSDI-Inputs-as-Outputs/m-p/1321332#M11762</link>
      <description>&lt;P&gt;This is regarding the Multi Switch Detector Interface ICs.&lt;/P&gt;&lt;P&gt;On the datasheets for the MC33972, MC33975, MC34972 and MC34975, it's shown how the input wetting current supplies can be used like outputs to drive a small load like an LED.&lt;/P&gt;&lt;P&gt;On the datasheets for the MC33978, MC34978, CD1020 and CD1030, this application is not mentioned, but at a first glance it seems that there is no reason why these ICs wouldn't be able to do this as well. Is someone able to confirm that this works on these ICs too?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 10 Aug 2021 21:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MSDI-Inputs-as-Outputs/m-p/1321332#M11762</guid>
      <dc:creator>mark512</dc:creator>
      <dc:date>2021-08-10T21:09:52Z</dc:date>
    </item>
    <item>
      <title>Re: MSDI Inputs as Outputs</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MSDI-Inputs-as-Outputs/m-p/1323055#M11789</link>
      <description>&lt;P&gt;No problem for them(&lt;SPAN&gt;&amp;nbsp;MC33978, MC34978, CD1020 and CD1030&lt;/SPAN&gt;) to drive LED.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 07:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MSDI-Inputs-as-Outputs/m-p/1323055#M11789</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-08-13T07:24:22Z</dc:date>
    </item>
  </channel>
</rss>