<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Any updates on OCamCalib tool in i.MX Surround View System? in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1312298#M11611</link>
    <description>&lt;P&gt;Hi, Bio_TICFSL.&lt;/P&gt;&lt;P&gt;Is this malposition in the demo application using local video files normal?&lt;/P&gt;&lt;P&gt;Because I am not sure this is due to my calibration or I should modify the source code logic for generating the result 3d rendering view. The obvious malposition and ghosts are happening to the objects near the overlap seams region especially when one moves them far away from the center of the view or raises them higher.&lt;/P&gt;</description>
    <pubDate>Fri, 23 Jul 2021 02:58:50 GMT</pubDate>
    <dc:creator>3412</dc:creator>
    <dc:date>2021-07-23T02:58:50Z</dc:date>
    <item>
      <title>Any updates on OCamCalib tool in i.MX Surround View System?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1308247#M11523</link>
      <description>&lt;P&gt;&amp;nbsp; &amp;nbsp; My company is using&amp;nbsp;i.MX Surround View System on QNX system, which calibrates cameras by the &lt;EM&gt;OCamCalib&lt;/EM&gt; tools based on&lt;EM&gt; Scaramuzza&lt;/EM&gt;'s idea. I saw on the internet that &lt;EM&gt;Urban&lt;/EM&gt; has improved this algorithm (&lt;A href="https://github.com/urbste/ImprovedOcamCalib" target="_blank" rel="noopener"&gt;https://github.com/urbste/ImprovedOcamCalib&lt;/A&gt;). Because I always see misplacement and ghosts near the overlap regions in the demo using local video files and the app fed on cameras calibrated myself. I think maybe I need more precise calibration. I wonder if there's any update of the &lt;EM&gt;OCamCalib&lt;/EM&gt; tool or a way to apply &lt;EM&gt;Urban&lt;/EM&gt;'s algorithm. (The tool within the system only contains a executable file and the &lt;EM&gt;autoCornerFinder&lt;/EM&gt;&amp;nbsp;folder given by Scaramuzza. And I myself am not familiar with Matlab.)&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 08:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1308247#M11523</guid>
      <dc:creator>3412</dc:creator>
      <dc:date>2021-07-15T08:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: Any updates on OCamCalib tool in i.MX Surround View System?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1308455#M11528</link>
      <description>&lt;P&gt;Hello 3412,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no available Update for the OCamCalib since it works, you should try to contact the developers of Ocamcalib if they now about this function and they will update the tool.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 13:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1308455#M11528</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2021-07-15T13:31:51Z</dc:date>
    </item>
    <item>
      <title>Re: Any updates on OCamCalib tool in i.MX Surround View System?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1312298#M11611</link>
      <description>&lt;P&gt;Hi, Bio_TICFSL.&lt;/P&gt;&lt;P&gt;Is this malposition in the demo application using local video files normal?&lt;/P&gt;&lt;P&gt;Because I am not sure this is due to my calibration or I should modify the source code logic for generating the result 3d rendering view. The obvious malposition and ghosts are happening to the objects near the overlap seams region especially when one moves them far away from the center of the view or raises them higher.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jul 2021 02:58:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Any-updates-on-OCamCalib-tool-in-i-MX-Surround-View-System/m-p/1312298#M11611</guid>
      <dc:creator>3412</dc:creator>
      <dc:date>2021-07-23T02:58:50Z</dc:date>
    </item>
  </channel>
</rss>