<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TJA1042T/3 CAN Transceiver doesn't work in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309396#M11559</link>
    <description>&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;Thanks for the advice. As additional information &lt;SPAN&gt;Using STM32F407VG6 chip, &lt;BR /&gt;APB1 Clock was set to 24Mhz. &lt;BR /&gt;&lt;BR /&gt;Prescaler was set to 3, Time Quantum to 125.0ns, Bit Segment 1 to 13 Times, &lt;BR /&gt;and Bit Segment2 to 2 Times. As a result, we set the conditions of 500k bit/s, &lt;BR /&gt;sample point 87.5%.&lt;BR /&gt;&lt;BR /&gt;The PCAN settings were also set the same as above. Maybe my settings are wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/PRE&gt;</description>
    <pubDate>Sun, 18 Jul 2021 09:47:34 GMT</pubDate>
    <dc:creator>ldj979</dc:creator>
    <dc:date>2021-07-18T09:47:34Z</dc:date>
    <item>
      <title>TJA1042T/3 CAN Transceiver doesn't work</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309357#M11556</link>
      <description>&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;Dear NPX users,
nice to meet you.

I am a beginner designer using NXP products.

I designed the CAN Transceiver circuit by looking at the data sheet and application note of the NXP High Speed ​​CAN Transceiver TJA1042T/3 product suitable for 3.3V MCU.

Based on the completed circuit, a problem occurred during hardware debugging of the board and I have a question.

I know that high-speed CAN communication requires 3.5V and 1.5V of CAN H and CAN L signals, respectively, based on 2.5V. &lt;BR /&gt;&lt;BR /&gt;However, in the board I designed, although the 2.5V reference point is the same, there is a problem that CAN H and CAN L output 3.9V and 1.1V, respectively.

Currently, I set 500k/bps and 87.5% of Sample Point through PEAK System's CAN communication equipment.&lt;BR /&gt;&lt;BR /&gt;I checked the communication, but found the problem that communication was not working.&lt;BR /&gt; &lt;BR /&gt;I am judging that communication is not possible due to the above problem. &lt;BR /&gt;&lt;BR /&gt;I would like to hear from users if the circuit I designed is a badly designed circuit.&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Sat, 17 Jul 2021 13:24:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309357#M11556</guid>
      <dc:creator>ldj979</dc:creator>
      <dc:date>2021-07-17T13:24:43Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1042T/3 CAN Transceiver doesn't work</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309360#M11557</link>
      <description>&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;Additionally
CAN equipment is also equipped with a Termination Resistor.&lt;/SPAN&gt;&lt;/PRE&gt;&lt;DIV class="lia-progress-placeholder mceNonEditable"&gt;&lt;DIV class="lia-media-progress"&gt;&lt;DIV class="lia-progress-bar-stripes lia-progress-bar-animate lia-media-progress-bar"&gt;&lt;DIV class="lia-progress-bar"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class="lia-progress-value"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class="lia-progress-placeholder mceNonEditable"&gt;&lt;DIV class="lia-media-progress"&gt;&lt;DIV class="lia-progress-bar-stripes lia-progress-bar-animate lia-media-progress-bar"&gt;&lt;DIV class="lia-progress-bar"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;SPAN class="lia-progress-value"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;PRE&gt;&amp;nbsp;&lt;/PRE&gt;</description>
      <pubDate>Sat, 17 Jul 2021 13:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309360#M11557</guid>
      <dc:creator>ldj979</dc:creator>
      <dc:date>2021-07-17T13:34:21Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1042T/3 CAN Transceiver doesn't work</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309395#M11558</link>
      <description>&lt;P&gt;With 500kbps shortest time between two adjacent edges should be 2us. On your waveform it is something like 5-10us. Please check your CAN bus timing.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 18 Jul 2021 08:54:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309395#M11558</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2021-07-18T08:54:51Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1042T/3 CAN Transceiver doesn't work</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309396#M11559</link>
      <description>&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;Thanks for the advice. As additional information &lt;SPAN&gt;Using STM32F407VG6 chip, &lt;BR /&gt;APB1 Clock was set to 24Mhz. &lt;BR /&gt;&lt;BR /&gt;Prescaler was set to 3, Time Quantum to 125.0ns, Bit Segment 1 to 13 Times, &lt;BR /&gt;and Bit Segment2 to 2 Times. As a result, we set the conditions of 500k bit/s, &lt;BR /&gt;sample point 87.5%.&lt;BR /&gt;&lt;BR /&gt;The PCAN settings were also set the same as above. Maybe my settings are wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Sun, 18 Jul 2021 09:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309396#M11559</guid>
      <dc:creator>ldj979</dc:creator>
      <dc:date>2021-07-18T09:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1042T/3 CAN Transceiver doesn't work</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309607#M11565</link>
      <description>I'm not familiar with STM32. Having oscilloscope you always can confirm CAN bit timing. Waveform you presented doesn't look like 500kbps CAN.</description>
      <pubDate>Mon, 19 Jul 2021 06:44:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309607#M11565</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2021-07-19T06:44:27Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1042T/3 CAN Transceiver doesn't work</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309645#M11569</link>
      <description>&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;As a result of checking with your advice, &lt;BR /&gt;the external crystal frequency did not match and the bit timing seemed to be strange. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;I modified the crystal frequency and it works fine as a result.
thank you&lt;/SPAN&gt;&lt;/PRE&gt;&lt;PRE&gt;&lt;SPAN class="Y2IQFc"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/PRE&gt;</description>
      <pubDate>Mon, 19 Jul 2021 07:25:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1042T-3-CAN-Transceiver-doesn-t-work/m-p/1309645#M11569</guid>
      <dc:creator>ldj979</dc:creator>
      <dc:date>2021-07-19T07:25:28Z</dc:date>
    </item>
  </channel>
</rss>