<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックSC18IS602B I2C to SPI Bridge Latch-Up Issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS602B-I2C-to-SPI-Bridge-Latch-Up-Issue/m-p/1305978#M11482</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are facing&amp;nbsp;SC18IS602B I2C to SPI bridge Latch-Up issue after power down system (from S0-S5-G3).&lt;/P&gt;&lt;P&gt;The failure rate is around 0.26% (4pcs out of 1500pcs)&lt;/P&gt;&lt;P&gt;We take this part in Intel x86 platform to convert data from embedded controller&amp;nbsp;IT5121VG to battery charger&amp;nbsp;LTC1960CG#TRPBF (SS0#).&lt;/P&gt;&lt;P&gt;It was found the VDD(3.3V) has voltage remained (0.3V) during power off. It needs to take a time for fully discharging remained power.&lt;/P&gt;&lt;P&gt;The latch-up occurred after next power up with VDD remaining power 0.3V. The failure rate is not 100% but close to 10%.&lt;/P&gt;&lt;P&gt;Pulling RESET# signal to low cannot fix latch-up issue when problem occurred.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We would like to clarify some items:&lt;/P&gt;&lt;P&gt;1) What's the latch-up condition of this part ?&lt;/P&gt;&lt;P&gt;2) What's the voltage threshold of power on reset(POR) for this part ?&lt;/P&gt;</description>
    <pubDate>Mon, 12 Jul 2021 07:38:49 GMT</pubDate>
    <dc:creator>eltonwang</dc:creator>
    <dc:date>2021-07-12T07:38:49Z</dc:date>
    <item>
      <title>SC18IS602B I2C to SPI Bridge Latch-Up Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS602B-I2C-to-SPI-Bridge-Latch-Up-Issue/m-p/1305978#M11482</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are facing&amp;nbsp;SC18IS602B I2C to SPI bridge Latch-Up issue after power down system (from S0-S5-G3).&lt;/P&gt;&lt;P&gt;The failure rate is around 0.26% (4pcs out of 1500pcs)&lt;/P&gt;&lt;P&gt;We take this part in Intel x86 platform to convert data from embedded controller&amp;nbsp;IT5121VG to battery charger&amp;nbsp;LTC1960CG#TRPBF (SS0#).&lt;/P&gt;&lt;P&gt;It was found the VDD(3.3V) has voltage remained (0.3V) during power off. It needs to take a time for fully discharging remained power.&lt;/P&gt;&lt;P&gt;The latch-up occurred after next power up with VDD remaining power 0.3V. The failure rate is not 100% but close to 10%.&lt;/P&gt;&lt;P&gt;Pulling RESET# signal to low cannot fix latch-up issue when problem occurred.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We would like to clarify some items:&lt;/P&gt;&lt;P&gt;1) What's the latch-up condition of this part ?&lt;/P&gt;&lt;P&gt;2) What's the voltage threshold of power on reset(POR) for this part ?&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jul 2021 07:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IS602B-I2C-to-SPI-Bridge-Latch-Up-Issue/m-p/1305978#M11482</guid>
      <dc:creator>eltonwang</dc:creator>
      <dc:date>2021-07-12T07:38:49Z</dc:date>
    </item>
    <item>
      <title>Re: SC18IS602B I2C to SPI Bridge Latch-Up Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC18IS602B-I2C-to-SPI-Bridge-Latch-Up-Issue/m-p/1306376#M11485</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Latch-up depends on the pin configuration and the conditions are explained on sections 7.1.11.1, 7.1.11.2, 7.1.11.3 and 7.1.11.4 of the devices datasheet: &lt;A href="https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2. It is the HIGH-LOW threshold voltage of MIN = 0.22VDD and TYP.=0.4VDD.&lt;/P&gt;
&lt;P&gt;And LOW-HIGH threshold voltage of TYP = 0.6VDD and MAX = 0.7VDD&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jose&lt;/P&gt;</description>
      <pubDate>Mon, 12 Jul 2021 23:24:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC18IS602B-I2C-to-SPI-Bridge-Latch-Up-Issue/m-p/1306376#M11485</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2021-07-12T23:24:34Z</dc:date>
    </item>
  </channel>
</rss>