<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: LS1046A DDR4 support</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1299683#M11415</link>
    <description>&lt;P&gt;1. Yes, it does.&lt;/P&gt;
&lt;P&gt;2. No 'specific' connector types. On the LS1046RDB we use part number 78730-1002 from Molex.&lt;/P&gt;
&lt;P&gt;3, 4. No, we do not have LS1046A-based boards with two DIMMs, so did not test such configuration. Potentially it could be possible, however maximum working DDR frequency may be affected due to greater load.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 29 Jun 2021 12:16:30 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2021-06-29T12:16:30Z</dc:date>
    <item>
      <title>LS1046A DDR4 support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1299538#M11411</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;We are planning to use LS1046A processor for new design.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) Does Processor support 32GB DDR4 RAM?&lt;/P&gt;&lt;P&gt;2) Is there any specific type of DIMM connector defined by NxP for DDR? Is yes then, Please help to share the details for the same.&lt;/P&gt;&lt;P&gt;3) If it supports 32GB then can we give provision by using 2 DIMM slots for two 16GB DDR4 module?&lt;/P&gt;&lt;P&gt;4) Is they any reference design available with NxP which has support of two DIMM slots for the DDR4?&lt;/P&gt;&lt;P&gt;Please help to resolve above queries.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nimesh&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 08:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1299538#M11411</guid>
      <dc:creator>NimeshRana</dc:creator>
      <dc:date>2021-06-29T08:12:58Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1299683#M11415</link>
      <description>&lt;P&gt;1. Yes, it does.&lt;/P&gt;
&lt;P&gt;2. No 'specific' connector types. On the LS1046RDB we use part number 78730-1002 from Molex.&lt;/P&gt;
&lt;P&gt;3, 4. No, we do not have LS1046A-based boards with two DIMMs, so did not test such configuration. Potentially it could be possible, however maximum working DDR frequency may be affected due to greater load.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Bulat&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jun 2021 12:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1299683#M11415</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2021-06-29T12:16:30Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DDR4 support</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1766587#M20307</link>
      <description>&lt;P&gt;So can we confirm that&amp;nbsp;&lt;SPAN&gt;LS1046RDB&amp;nbsp;supports 32G DIMM DDR4?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 15:22:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DDR4-support/m-p/1766587#M20307</guid>
      <dc:creator>stefankolody</dc:creator>
      <dc:date>2023-11-30T15:22:01Z</dc:date>
    </item>
  </channel>
</rss>