<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: NFC For Windows Hello</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1290235#M11262</link>
    <description>&lt;P&gt;Hi Fabian,&amp;nbsp;&lt;/P&gt;&lt;P&gt;All we want to do is use the card to log into the PC using Windows 10.&amp;nbsp; No third party applications or additional hardware. We want to use a passive NFC credential to unlock the PC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Joseph&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jun 2021 22:12:05 GMT</pubDate>
    <dc:creator>TexasRFGuy</dc:creator>
    <dc:date>2021-06-09T22:12:05Z</dc:date>
    <item>
      <title>NFC For Windows Hello</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1283570#M11160</link>
      <description>&lt;P&gt;I am using the NXP7462 and am looking for a passive NFC tag that will work for Multi Factor Authentication using Windows Hello (Windows 10). Can anyone recommend a passive NFC tag?&amp;nbsp; I cant seem to find requirements and configuration instructions for Windows Hello using NFC.&amp;nbsp; Any help would be appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 27 May 2021 14:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1283570#M11160</guid>
      <dc:creator>TexasRFGuy</dc:creator>
      <dc:date>2021-05-27T14:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: NFC For Windows Hello</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1285634#M11202</link>
      <description>&lt;P&gt;Hope you are doing great, &lt;BR /&gt;In this case we need more information about the application of the tag in your system, do you want to use some NDEF capabilities?&lt;/P&gt;
&lt;P&gt;Do you need encryption? Do you want to use the card to login into a PC? The more details you can provide the best recommendation we can make. &lt;BR /&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 21:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1285634#M11202</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2021-06-01T21:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: NFC For Windows Hello</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1286899#M11221</link>
      <description>&lt;P&gt;Hi Fabian,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have a customer that is using Windows 10 and wants to use NFC to login to the computer. Encryption is preferred if Microsoft supports it but not required if they don't. With regards to NDEF capabilities, I am not sure about that one. The major requirement is that it must be supported by MS Windows Hello.&amp;nbsp; &amp;nbsp;As far as physical form factor we would like to use a sticker approximately 1 inch in diameter.&amp;nbsp; something similar to&amp;nbsp;&lt;A href="https://store.gototags.com/on-metal-nfc-sticker-ntag213-30-mm-circle/" target="_blank"&gt;https://store.gototags.com/on-metal-nfc-sticker-ntag213-30-mm-circle/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 14:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1286899#M11221</guid>
      <dc:creator>TexasRFGuy</dc:creator>
      <dc:date>2021-06-03T14:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: NFC For Windows Hello</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1290235#M11262</link>
      <description>&lt;P&gt;Hi Fabian,&amp;nbsp;&lt;/P&gt;&lt;P&gt;All we want to do is use the card to log into the PC using Windows 10.&amp;nbsp; No third party applications or additional hardware. We want to use a passive NFC credential to unlock the PC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Joseph&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 22:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NFC-For-Windows-Hello/m-p/1290235#M11262</guid>
      <dc:creator>TexasRFGuy</dc:creator>
      <dc:date>2021-06-09T22:12:05Z</dc:date>
    </item>
  </channel>
</rss>