<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC-LS-VNP-RDB 100Base-T1 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC-LS-VNP-RDB-100Base-T1/m-p/1288654#M11244</link>
    <description>&lt;P&gt;&lt;SPAN class="transSent"&gt;Hello, I want to realize network communication on the MPC-LS-VNP-RDB reference board. After I get the new reference board, I rewrote the system and set the system to start from EMMC. By configoring the network port IP, the network port of RJ45 on the board (Eth1,Eth4,Eth5,Eth6) can all communicate.&lt;/SPAN&gt;&lt;SPAN class="transSent"&gt;The configuration is shown below, but the on-board Ethernet does not communicate.&lt;/SPAN&gt;&lt;SPAN class="transSent"&gt;In general, eth1-1g can also connect to SJA1105, it can communicate, which means that the configuration of SJA1105 is good, but 100BASE-T1 can not communicate, I don't know why?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Jun 2021 02:43:16 GMT</pubDate>
    <dc:creator>babay1996</dc:creator>
    <dc:date>2021-06-08T02:43:16Z</dc:date>
    <item>
      <title>MPC-LS-VNP-RDB 100Base-T1</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC-LS-VNP-RDB-100Base-T1/m-p/1288654#M11244</link>
      <description>&lt;P&gt;&lt;SPAN class="transSent"&gt;Hello, I want to realize network communication on the MPC-LS-VNP-RDB reference board. After I get the new reference board, I rewrote the system and set the system to start from EMMC. By configoring the network port IP, the network port of RJ45 on the board (Eth1,Eth4,Eth5,Eth6) can all communicate.&lt;/SPAN&gt;&lt;SPAN class="transSent"&gt;The configuration is shown below, but the on-board Ethernet does not communicate.&lt;/SPAN&gt;&lt;SPAN class="transSent"&gt;In general, eth1-1g can also connect to SJA1105, it can communicate, which means that the configuration of SJA1105 is good, but 100BASE-T1 can not communicate, I don't know why?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jun 2021 02:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC-LS-VNP-RDB-100Base-T1/m-p/1288654#M11244</guid>
      <dc:creator>babay1996</dc:creator>
      <dc:date>2021-06-08T02:43:16Z</dc:date>
    </item>
  </channel>
</rss>