<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Alternate Request in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Alternate-Request/m-p/1287618#M11231</link>
    <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Hi,&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;We are using the parts&amp;nbsp;PTN3460BS/F6Y and&amp;nbsp;PTN3460BS/F4Y in our projects, Due to unavailability issue of these two parts , we are checking the part&amp;nbsp;PTN3460BS/F3 use as alternate for same project,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;we could see the below mentioned major points new feature when checking the release note of&amp;nbsp;PTN3460BS/F4Y,&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;*Implement DP one/two lane configurable setting in the configuration table (0x80 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;bit 2). &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;* Implement DP HRB/RBR or RBR only link rate configurable setting in the &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;configuration table (0x80 bit 3).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;*Fix the backlight control function in the configuration table (0x95 bit 0) may not &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;work while system logout and log back in. &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;*Increase FW PLL range to +/- 6.25%.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;I would like to get the full description of registers&amp;nbsp;0x95 and&amp;nbsp;0x80 for our reference and confirm to use as alternate , please share the description manual of&amp;nbsp;above mentioned registers.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Also , I noticed from PTN3460, PTN3460I FAQs page in nxp community product form, that FW can be updated by flash over I2C , can you please confirm whether we can use the part&amp;nbsp;TN3460BS/F3 as alternate for&amp;nbsp;PTN3460BS/F6Y by update the firmware flash over I2C?.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Thanks,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Jabir&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Jun 2021 14:36:45 GMT</pubDate>
    <dc:creator>Jab_1</dc:creator>
    <dc:date>2021-06-04T14:36:45Z</dc:date>
    <item>
      <title>Alternate Request</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Alternate-Request/m-p/1287618#M11231</link>
      <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Hi,&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;We are using the parts&amp;nbsp;PTN3460BS/F6Y and&amp;nbsp;PTN3460BS/F4Y in our projects, Due to unavailability issue of these two parts , we are checking the part&amp;nbsp;PTN3460BS/F3 use as alternate for same project,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;we could see the below mentioned major points new feature when checking the release note of&amp;nbsp;PTN3460BS/F4Y,&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;*Implement DP one/two lane configurable setting in the configuration table (0x80 &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;bit 2). &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;* Implement DP HRB/RBR or RBR only link rate configurable setting in the &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;configuration table (0x80 bit 3).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;*Fix the backlight control function in the configuration table (0x95 bit 0) may not &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;work while system logout and log back in. &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;*Increase FW PLL range to +/- 6.25%.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;I would like to get the full description of registers&amp;nbsp;0x95 and&amp;nbsp;0x80 for our reference and confirm to use as alternate , please share the description manual of&amp;nbsp;above mentioned registers.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Also , I noticed from PTN3460, PTN3460I FAQs page in nxp community product form, that FW can be updated by flash over I2C , can you please confirm whether we can use the part&amp;nbsp;TN3460BS/F3 as alternate for&amp;nbsp;PTN3460BS/F6Y by update the firmware flash over I2C?.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Thanks,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="2"&gt;Jabir&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jun 2021 14:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Alternate-Request/m-p/1287618#M11231</guid>
      <dc:creator>Jab_1</dc:creator>
      <dc:date>2021-06-04T14:36:45Z</dc:date>
    </item>
    <item>
      <title>Re: Alternate Request</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Alternate-Request/m-p/1288848#M11245</link>
      <description>&lt;P&gt;Hello Jabir,&lt;/P&gt;
&lt;P&gt;Please see the answers inserted below in your text.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;*Implement DP one/two lane configurable setting in the configuration table (0x80 bit 2).&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt; If configuration register 0x80 bit 2 = 0, then PTN3460 will report to support DP 2 lanes configuration in the DPCD register 0x0002.&lt;/P&gt;
&lt;P&gt;If configuration register 0x80 bit 2 = 1, then PTN3460 will report to support DP 1 lanes configuration in the DPCD register 0x0002.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;* Implement DP HRB/RBR or RBR only link rate configurable setting in the configuration table (0x80 bit 3).&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt; If configuration register 0x80 bit 3 = 0, then PTN3460 will report to support HBR (2.7Gbps) as max link rate in the DPCD register 0x0001.&lt;/P&gt;
&lt;P&gt;If configuration register 0x80 bit 3 = 1, then PTN3460 will report to support RBR (1.62Gbps) as max link rate in the DPCD register 0x0001.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;* Fix the backlight control function in the configuration table (0x95 bit 0) may not work while system logout and log back in.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt; if Configuration register 0x95 bit 0 = 0, then LCD backlight is ON.&lt;/P&gt;
&lt;P&gt;If Configuration register 0x95 bit 0 = 1, then LCD backlight is OFF.&lt;/P&gt;
&lt;P&gt;Users can use this bit to turn ON/OFF LCD backlight according to application needs, or just let PTN3460 control it in panel power on/off sequence.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;*Increase FW PLL range to +/- 6.25%.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt; It is for fast detection DP link lost and turn off LCD panel backlight in time. So as long as incoming pixel clock is out of +/-6.25%, then PTN3460 will decide that DP link is lost (or unstable), and turn off LCD panel backlight, so that user will not see garbage video on LCD panel.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;I would like to get the full description of registers 0x95 and 0x80 for our reference and confirm to use as alternate, please share the description manual of above mentioned registers.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Also, I noticed that FW can be updated by flash over I2C , can you please confirm whether we can use the part TN3460BS/F3 as alternate for PTN3460BS/F6Y by update the firmware flash over I2C?&lt;/EM&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;&amp;gt;&amp;gt; Yes, it should possible, you should get more information on that in your case #00372681.&lt;/P&gt;
&lt;P data-unlink="true"&gt;&amp;nbsp;&lt;/P&gt;
&lt;P data-unlink="true"&gt;Best regards,&lt;/P&gt;
&lt;P data-unlink="true"&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jun 2021 07:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Alternate-Request/m-p/1288848#M11245</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-06-08T07:42:03Z</dc:date>
    </item>
  </channel>
</rss>