<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックLPCLink2 + LPCXpresso</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LPCLink2-LPCXpresso/m-p/1275001#M11053</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have problem with LPC-Link2 on my Windows 10 computer. When I connect the programmer to my computer I can see it recognized in device manager and in LPCXpresso, but it does nothing on output (SWDIO, SWCLK are still in high),... I am not able to find programmer in MCUXpresso.&lt;/P&gt;&lt;P&gt;Error from LPCXpresso v8.2.2:&lt;/P&gt;&lt;P&gt;Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink.exe build 725)&lt;BR /&gt;Pc: ( 0) Reading remote configuration&lt;BR /&gt;Pc: ( 5) Remote configuration complete&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: probe unbooted? no core 0?&lt;BR /&gt;Ed:02: Failed on connect: Ee(36). Could not connect to core.&lt;BR /&gt;Et:31: No connection to emulator device&lt;BR /&gt;Pc: (100) Target Connection Failed&lt;/P&gt;&lt;P&gt;I tried driver and studio reinstall.&lt;/P&gt;</description>
    <pubDate>Tue, 11 May 2021 12:50:11 GMT</pubDate>
    <dc:creator>ELKO_EP</dc:creator>
    <dc:date>2021-05-11T12:50:11Z</dc:date>
    <item>
      <title>LPCLink2 + LPCXpresso</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LPCLink2-LPCXpresso/m-p/1275001#M11053</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have problem with LPC-Link2 on my Windows 10 computer. When I connect the programmer to my computer I can see it recognized in device manager and in LPCXpresso, but it does nothing on output (SWDIO, SWCLK are still in high),... I am not able to find programmer in MCUXpresso.&lt;/P&gt;&lt;P&gt;Error from LPCXpresso v8.2.2:&lt;/P&gt;&lt;P&gt;Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink.exe build 725)&lt;BR /&gt;Pc: ( 0) Reading remote configuration&lt;BR /&gt;Pc: ( 5) Remote configuration complete&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: connecting to core 0 with handle 0x0 (using server PID -1) gave rc 'Ee(36). Could not connect to core.'&lt;BR /&gt;Nc: probe unbooted? no core 0?&lt;BR /&gt;Ed:02: Failed on connect: Ee(36). Could not connect to core.&lt;BR /&gt;Et:31: No connection to emulator device&lt;BR /&gt;Pc: (100) Target Connection Failed&lt;/P&gt;&lt;P&gt;I tried driver and studio reinstall.&lt;/P&gt;</description>
      <pubDate>Tue, 11 May 2021 12:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LPCLink2-LPCXpresso/m-p/1275001#M11053</guid>
      <dc:creator>ELKO_EP</dc:creator>
      <dc:date>2021-05-11T12:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPCLink2 + LPCXpresso</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LPCLink2-LPCXpresso/m-p/1276486#M11073</link>
      <description>&lt;P&gt;Hello ELKO_EP,&lt;/P&gt;
&lt;P&gt;Would you please provide more information on the target you want to debug?&lt;/P&gt;
&lt;P&gt;I would recommend tying to set the target to ISP mode. The LPC-Link2 has the ability to force an ISP reset but I would recommend making sure the connections are setup for this. You can find more details on the link below:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565" target="_blank"&gt;https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 16:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LPCLink2-LPCXpresso/m-p/1276486#M11073</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2021-05-13T16:03:39Z</dc:date>
    </item>
  </channel>
</rss>