<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: FS32R274KBK2MMM BootLoader erro</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267831#M10965</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;the second part number doesn't seem to be correct one. Could you send me a photo of the chip?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Mon, 26 Apr 2021 05:30:58 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2021-04-26T05:30:58Z</dc:date>
    <item>
      <title>FS32R274KBK2MMM BootLoader erro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267719#M10964</link>
      <description>&lt;P&gt;&lt;SPAN class="VIiyi"&gt;&lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;I tested the BootLoader on FS32R274KSK2MMM and used software reset to update the APP without any problems. When I test the same BootLoader code on FS32R274KBMMM2N58R there will be a high probability of error and update failure. Compare the difference between the two. X has more CSE modules than Y, but I&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class="JLqJ4b ChMk0b"&gt;&lt;SPAN&gt;The CSE module is not used in BootLoader.Do I need to make some changes on BootLoader to avoid this update failure problem?&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 01:48:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267719#M10964</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-04-26T01:48:09Z</dc:date>
    </item>
    <item>
      <title>Re: FS32R274KBK2MMM BootLoader erro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267831#M10965</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;the second part number doesn't seem to be correct one. Could you send me a photo of the chip?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 05:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267831#M10965</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-04-26T05:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: FS32R274KBK2MMM BootLoader erro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267885#M10966</link>
      <description>&lt;P&gt;Sorry K2&amp;nbsp; is&amp;nbsp; error,The silk&amp;nbsp; is shown in the picture below&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="FS32R274KBK2MMM.jpg" style="width: 939px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/143196i822B9DD564B3CBDC/image-size/large?v=v2&amp;amp;px=999" role="button" title="FS32R274KBK2MMM.jpg" alt="FS32R274KBK2MMM.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 06:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1267885#M10966</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-04-26T06:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: FS32R274KBK2MMM BootLoader erro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1268194#M10969</link>
      <description>&lt;P&gt;Thanks for the details.&lt;BR /&gt;So, we have two ordering part numbers:&lt;BR /&gt;FS32R274KSK2MMM&lt;BR /&gt;FS32R274KBK2MMM&lt;/P&gt;
&lt;P&gt;According to marking diagram, mask set (‘K2’) is omitted in the printing on the package due to space constraints, so there’s only:&lt;BR /&gt;FS32R274KSMMM&lt;BR /&gt;FS32R274KBMMM&lt;BR /&gt;… and the mask set is shown below the part number as 2N58R.&lt;/P&gt;
&lt;P&gt;These are exactly the same devices with the same silicon mask set. CSE is available in both versions. ‘S’ and ‘B’ is used only due to some historical reasons. I got confirmation there's no difference at all.&lt;/P&gt;
&lt;P&gt;It would be necessary to have more details about the failure. Isn’t it somehow related to (other) hardware?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 26 Apr 2021 13:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1268194#M10969</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-04-26T13:33:22Z</dc:date>
    </item>
    <item>
      <title>Re: FS32R274KBK2MMM BootLoader erro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1268668#M10971</link>
      <description>&lt;P&gt;The schematic is the same, but the PCB layout is different.&lt;/P&gt;&lt;P&gt;The FS32R274KSMMM is powered off when updating the APP, and reading the flash at the next power-on will generate an ECC error and enter the IVOR1 interrupt.FS32R274KBMMM &amp;nbsp;reading flash can also generate ECC error&amp;nbsp;But cannot enter IVOR1 interrupt.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 07:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1268668#M10971</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-04-27T07:49:01Z</dc:date>
    </item>
    <item>
      <title>Re: FS32R274KBK2MMM BootLoader erro</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1269360#M10981</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;isn't the flash corrupted in another way? This could be the source of troubles. Have you checked the content of flash by a debugger? Does IVPR register contain expected value? Is IVOR1 still there? Isn't it erased? IVOR1 is not maskable in case of ECC double it error, so I would check what really happened at the beginning.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 06:06:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FS32R274KBK2MMM-BootLoader-erro/m-p/1269360#M10981</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2021-04-28T06:06:05Z</dc:date>
    </item>
  </channel>
</rss>