<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPCA2129 problem in OSF value</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA2129-problem-in-OSF-value/m-p/1252068#M10719</link>
    <description>&lt;P&gt;hello .&lt;/P&gt;&lt;P&gt;I have a problem when i read seconds register of PCA2129 the osf bit is always 1 so that make my recieved data are not right so can you please tell me how to set that bit 0 ?? or what should i do to solve this problem so osf would not be 1&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using SPI protocol in TMS570LS07 mcu with PCA2129 and I am sending&amp;nbsp;TX_DATA[0]=0xA3;to read seconds register&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uint16_t TX_DATA[100];&lt;BR /&gt;uint16_t RX_DATA[100];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;uint8_t readsecondsRegister() {&lt;BR /&gt;gioSetBit(spiPORT1, 0U, 0);&lt;BR /&gt;TX_DATA[0]=0xA3;&lt;BR /&gt;spiTransmitData(spiREG1, &amp;amp;dataconfig1_t, 1, (uint16_t*)&amp;amp;TX_DATA[0]);&lt;BR /&gt;spiReceiveData(spiREG1, &amp;amp;dataconfig1_t, 1, (uint16_t*)&amp;amp;RX_DATA[0]);&lt;BR /&gt;gioSetBit(spiPORT1, 0U, 1);&lt;BR /&gt;return (uint8_t)RX_DATA[0];&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 25 Mar 2021 10:21:18 GMT</pubDate>
    <dc:creator>mouaiadsalaas</dc:creator>
    <dc:date>2021-03-25T10:21:18Z</dc:date>
    <item>
      <title>PCA2129 problem in OSF value</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA2129-problem-in-OSF-value/m-p/1252068#M10719</link>
      <description>&lt;P&gt;hello .&lt;/P&gt;&lt;P&gt;I have a problem when i read seconds register of PCA2129 the osf bit is always 1 so that make my recieved data are not right so can you please tell me how to set that bit 0 ?? or what should i do to solve this problem so osf would not be 1&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using SPI protocol in TMS570LS07 mcu with PCA2129 and I am sending&amp;nbsp;TX_DATA[0]=0xA3;to read seconds register&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uint16_t TX_DATA[100];&lt;BR /&gt;uint16_t RX_DATA[100];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;uint8_t readsecondsRegister() {&lt;BR /&gt;gioSetBit(spiPORT1, 0U, 0);&lt;BR /&gt;TX_DATA[0]=0xA3;&lt;BR /&gt;spiTransmitData(spiREG1, &amp;amp;dataconfig1_t, 1, (uint16_t*)&amp;amp;TX_DATA[0]);&lt;BR /&gt;spiReceiveData(spiREG1, &amp;amp;dataconfig1_t, 1, (uint16_t*)&amp;amp;RX_DATA[0]);&lt;BR /&gt;gioSetBit(spiPORT1, 0U, 1);&lt;BR /&gt;return (uint8_t)RX_DATA[0];&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Mar 2021 10:21:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA2129-problem-in-OSF-value/m-p/1252068#M10719</guid>
      <dc:creator>mouaiadsalaas</dc:creator>
      <dc:date>2021-03-25T10:21:18Z</dc:date>
    </item>
  </channel>
</rss>