<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with programming NHS3100 via Flash Magic in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-programming-NHS3100-via-Flash-Magic/m-p/1248442#M10642</link>
    <description>&lt;P&gt;I'm trying to flash firmware image in Intel HEX format to NHS3100 connected with the LPC-Link2 board and it fails with warning: &lt;STRONG&gt;"NHS3100 (SWD, NHS3100) Unable to open Hex file. Reselect the Hex file"&lt;/STRONG&gt;. I'm sure, that all is correctly connected and I choose options in Flash Magic as it's shown in the &lt;EM&gt;UM11154&lt;/EM&gt; document (in NHS3100 SDK) and screen is attached. Why is this issue present?&lt;/P&gt;&lt;P&gt;There are screenshots of the Device Manager window in attachments where you can clearly see issues with drivers. I think that it could have affected on the issue in Flash Magic. But I'm not sure about it.&lt;/P&gt;</description>
    <pubDate>Fri, 19 Mar 2021 00:00:27 GMT</pubDate>
    <dc:creator>pilot_art_lis</dc:creator>
    <dc:date>2021-03-19T00:00:27Z</dc:date>
    <item>
      <title>Problem with programming NHS3100 via Flash Magic</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-programming-NHS3100-via-Flash-Magic/m-p/1248442#M10642</link>
      <description>&lt;P&gt;I'm trying to flash firmware image in Intel HEX format to NHS3100 connected with the LPC-Link2 board and it fails with warning: &lt;STRONG&gt;"NHS3100 (SWD, NHS3100) Unable to open Hex file. Reselect the Hex file"&lt;/STRONG&gt;. I'm sure, that all is correctly connected and I choose options in Flash Magic as it's shown in the &lt;EM&gt;UM11154&lt;/EM&gt; document (in NHS3100 SDK) and screen is attached. Why is this issue present?&lt;/P&gt;&lt;P&gt;There are screenshots of the Device Manager window in attachments where you can clearly see issues with drivers. I think that it could have affected on the issue in Flash Magic. But I'm not sure about it.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 00:00:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-programming-NHS3100-via-Flash-Magic/m-p/1248442#M10642</guid>
      <dc:creator>pilot_art_lis</dc:creator>
      <dc:date>2021-03-19T00:00:27Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with programming NHS3100 via Flash Magic</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-programming-NHS3100-via-Flash-Magic/m-p/1249198#M10667</link>
      <description>&lt;P&gt;I've found the solution. The path's name was a problem. HEX files I wanted to load to NHS3100 with Flash Magic were situated in the Desktop and my username was in the path. &lt;STRONG&gt;Username was written in cyrillic&lt;/STRONG&gt; and the program had problems with it. &lt;EM&gt;When I moved test files to the folder on the disk C:\ (where username isn't in path) it worked!&lt;/EM&gt; Flash Magic could program NHS3100 successfully.&lt;/P&gt;&lt;P&gt;I hope my experience could help someone and don't lose some days to find the solution.&lt;/P&gt;</description>
      <pubDate>Sun, 21 Mar 2021 15:45:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-with-programming-NHS3100-via-Flash-Magic/m-p/1249198#M10667</guid>
      <dc:creator>pilot_art_lis</dc:creator>
      <dc:date>2021-03-21T15:45:12Z</dc:date>
    </item>
  </channel>
</rss>