<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problems with NX3L4051 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-NX3L4051/m-p/1230710#M10436</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;For my bachelor thesis I use the multiplexer NX3L4051. Now I have the problem that I have not taken into account the internal protective circuit. Thus my circuit does not work as intended.&lt;/P&gt;&lt;P&gt;Briefly to the function: I would like to implement a ratiometric resistance measurement. For this I have several reference resistors at the inputs of the NX3L4051 (Y0, Y1,...). These I have connected to a 5V reference voltage, by the internal protection circuit is now a current in my measurement imprinted that I do not want. Could you give me a sketch of the internal circuit, so I can think of a circuit how I can still save my PCB.&lt;/P&gt;&lt;P&gt;And I connect the unknown resistor to GND at the output of the NX3L4051 (output Z) and measure the voltage with an ADC.&lt;/P&gt;&lt;P&gt;Do you have a multiplexer that has the same pin layout but can handle up to 5V at the inputs ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;</description>
    <pubDate>Sat, 13 Feb 2021 13:18:51 GMT</pubDate>
    <dc:creator>Drops93</dc:creator>
    <dc:date>2021-02-13T13:18:51Z</dc:date>
    <item>
      <title>Problems with NX3L4051</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-NX3L4051/m-p/1230710#M10436</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;For my bachelor thesis I use the multiplexer NX3L4051. Now I have the problem that I have not taken into account the internal protective circuit. Thus my circuit does not work as intended.&lt;/P&gt;&lt;P&gt;Briefly to the function: I would like to implement a ratiometric resistance measurement. For this I have several reference resistors at the inputs of the NX3L4051 (Y0, Y1,...). These I have connected to a 5V reference voltage, by the internal protection circuit is now a current in my measurement imprinted that I do not want. Could you give me a sketch of the internal circuit, so I can think of a circuit how I can still save my PCB.&lt;/P&gt;&lt;P&gt;And I connect the unknown resistor to GND at the output of the NX3L4051 (output Z) and measure the voltage with an ADC.&lt;/P&gt;&lt;P&gt;Do you have a multiplexer that has the same pin layout but can handle up to 5V at the inputs ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;</description>
      <pubDate>Sat, 13 Feb 2021 13:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-NX3L4051/m-p/1230710#M10436</guid>
      <dc:creator>Drops93</dc:creator>
      <dc:date>2021-02-13T13:18:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with NX3L4051</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-NX3L4051/m-p/1230872#M10439</link>
      <description>&lt;P&gt;Hi Jan,&lt;/P&gt;
&lt;P&gt;The max recommended supply voltage is 4.3V and the&amp;nbsp;switching voltage should not be higher than VCC.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 6.JPG" style="width: 673px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137171iD6548A640F401BF8/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 6.JPG" alt="Table 6.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Table 6.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Back power, voltage swing limited, may happen when Vsw &amp;gt; Vcc, basically due to ESD diode may be turning on.&lt;/P&gt;
&lt;P&gt;We do not have any pin compatible multiplexes capable to handle up to 5V at the inputs.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 15 Feb 2021 08:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problems-with-NX3L4051/m-p/1230872#M10439</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-02-15T08:26:22Z</dc:date>
    </item>
  </channel>
</rss>