<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NXP B4860QDS J2 debug port in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1208781#M10174</link>
    <description>&lt;P&gt;We have 2 boards. One is working with eCWTAP, and the second is not.&amp;nbsp; Both have the same RCW. On the second board D1 and D2 LEDs do not lit and the LEDs on CWTAP Ethernet port do not lit also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 14000e18 0f001218 00000000 00000000&lt;BR /&gt;00000010: 528c0000 a000a000 ec025000 a9000000&lt;BR /&gt;00000020: 01000000 00000000 00000000 0001b1f8&lt;BR /&gt;00000030: 00000000 14000020 00000000 00000011&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 14000e18 0f001218 00000000 00000000&lt;BR /&gt;00000010: 528c0000 a000a000 ec025000 a9000000&lt;BR /&gt;00000020: 01000000 00000000 00000000 0001b1f8&lt;BR /&gt;00000030: 00000000 14000020 00000000 00000011&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jan 2021 08:02:20 GMT</pubDate>
    <dc:creator>apush</dc:creator>
    <dc:date>2021-01-08T08:02:20Z</dc:date>
    <item>
      <title>NXP B4860QDS J2 debug port</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1202338#M10078</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I have a basic connectivity problem with my NXP B4860QDS J2 debug port.&lt;BR /&gt;&lt;BR /&gt;I have closely followed the “Quick Start Guide for B4860QDS and B4420QDS” and I believe that all configurations and connections are made correctly and using only the hardware kit contents supplied.&lt;/P&gt;&lt;P&gt;However, after powering on the board, there is a problem with the J2 USB debug/eCWTAP connectivity as follows:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;D1 (eCWTAP) LED is not lit at any time – neither orange nor green is observed. This suggests that eCWTAP is inactive.&lt;/LI&gt;&lt;LI&gt;Using both Linux Ubuntu 18.04 and Windows 10 operating systems and 2 different cables, no connectivity is detected on either PC USB port at any time.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;This problem is fully repeatable.&lt;BR /&gt;&lt;BR /&gt;Attached are photos&amp;nbsp;showing:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Jumper Settings – set as default (J21 with CLOSE: 2-3)&lt;/LI&gt;&lt;LI&gt;DIP-Switch Settings – set as default (SW1, SW2, SW3, SW5)&lt;/LI&gt;&lt;LI&gt;LEDs (D1 is not lit)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Please could you suggest as to why the J2/D1 USB debug connectivity is not working as expected.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Dec 2020 08:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1202338#M10078</guid>
      <dc:creator>sread</dc:creator>
      <dc:date>2020-12-21T08:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: NXP B4860QDS J2 debug port</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1202973#M10092</link>
      <description>&lt;P&gt;Please refer to CodeWarrior_PA_10.5.1/PA/ccs/drivers/usb/readme.cwtap.txt to install the &lt;STRONG&gt;udev&lt;/STRONG&gt; rule and make it take effective on your Linux host PC.&lt;/P&gt;
&lt;P&gt;NOR_BOOT switch setting.&lt;BR /&gt;---------&lt;/P&gt;
&lt;P&gt;SW1 : 0x00 = 00000000 SW2 : 0xFC = 11111100 SW3 : 0x12 = 00010010&lt;BR /&gt;SW5 : 0x03 = 00000011&lt;/P&gt;
&lt;P&gt;If there is no valid RCW on the target board, please use hard-coded RCW.&lt;/P&gt;
&lt;P&gt;Please open CCS console and type the following command.&lt;/P&gt;
&lt;P&gt;(bin) 5 % findcc cwtaps&lt;BR /&gt;FSL02F1EA (00:04:9f:02:f1:ea): CodeWarrior TAP&lt;BR /&gt;Unknown probe (ID 2) Probe Tip&lt;BR /&gt;Boot Loader v1.0.1&lt;BR /&gt;Operating System v1.0.1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 08:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1202973#M10092</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-12-22T08:50:15Z</dc:date>
    </item>
    <item>
      <title>Re: NXP B4860QDS J2 debug port</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1208781#M10174</link>
      <description>&lt;P&gt;We have 2 boards. One is working with eCWTAP, and the second is not.&amp;nbsp; Both have the same RCW. On the second board D1 and D2 LEDs do not lit and the LEDs on CWTAP Ethernet port do not lit also.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 14000e18 0f001218 00000000 00000000&lt;BR /&gt;00000010: 528c0000 a000a000 ec025000 a9000000&lt;BR /&gt;00000020: 01000000 00000000 00000000 0001b1f8&lt;BR /&gt;00000030: 00000000 14000020 00000000 00000011&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 14000e18 0f001218 00000000 00000000&lt;BR /&gt;00000010: 528c0000 a000a000 ec025000 a9000000&lt;BR /&gt;00000020: 01000000 00000000 00000000 0001b1f8&lt;BR /&gt;00000030: 00000000 14000020 00000000 00000011&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 08:02:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1208781#M10174</guid>
      <dc:creator>apush</dc:creator>
      <dc:date>2021-01-08T08:02:20Z</dc:date>
    </item>
    <item>
      <title>Re: NXP B4860QDS J2 debug port</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1208956#M10180</link>
      <description>&lt;P&gt;We can't use CSS console, as CWTAP USB\Ethetnet port does not work at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;The first working board
~$ lsusb
Bus 002 Device 002: ID 8087:8000 Intel Corp. 
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 8087:8008 Intel Corp. 
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 004 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 003 Device 005: ID 8087:07dc Intel Corp. 
Bus 003 Device 004: ID 5986:0295 Acer, Inc 
Bus 003 Device 003: ID 058f:6366 Alcor Micro Corp. Multi Flash Reader
Bus 003 Device 013: ID 24ae:2000  
Bus 003 Device 012: ID 15a2:0067 Freescale Semiconductor, Inc. 
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

The second non-working board
~$ lsusb
Bus 002 Device 002: ID 8087:8000 Intel Corp. 
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 8087:8008 Intel Corp. 
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 004 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 003 Device 005: ID 8087:07dc Intel Corp. 
Bus 003 Device 004: ID 5986:0295 Acer, Inc 
Bus 003 Device 003: ID 058f:6366 Alcor Micro Corp. Multi Flash Reader
Bus 003 Device 013: ID 24ae:2000  
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 13:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXP-B4860QDS-J2-debug-port/m-p/1208956#M10180</guid>
      <dc:creator>apush</dc:creator>
      <dc:date>2021-01-08T13:19:19Z</dc:date>
    </item>
  </channel>
</rss>