<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: LS1046A DPDK l3fwd problem</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204795#M10120</link>
    <description>&lt;P&gt;l3fwd, as it's name suggests, uses L3 headers to make forwarding decisions.&lt;BR /&gt;The L3 protocols it supports are IPv4 and IPv6. This software is not suited for&lt;BR /&gt;handling other types of protocols, such as ARP, which is not strictly L3 or&lt;BR /&gt;EtherCAT which is L2. If you wish to handle other types of protocols, you &lt;BR /&gt;probably need to look at different DPDK applications or even create your own&lt;BR /&gt;from scratch. Everything depends on how you actually want to handle your ingress&lt;BR /&gt;egress traffic. If the task is just to make the node transparent to ARP,&lt;BR /&gt;you can take a look at l2fwd. As of EtherCAT, there is no support to it in &lt;BR /&gt;DPDK or LSDK at all.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;</description>
    <pubDate>Tue, 29 Dec 2020 07:46:15 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2020-12-29T07:46:15Z</dc:date>
    <item>
      <title>LS1046A DPDK l3fwd problem</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204069#M10107</link>
      <description>&lt;P&gt;I use the LS1046A to run DPDK example--l3fwd, the board can receive IP packets, it can also receive another Ethernet type packets, however, it will drop the packet excepted IP packet. I can not handle the other type of Ethernet packets. Shall I add the Ethernet type to a table in the program? where can I add the Ethernet type? Even the ARP can not be handled in the program. I want to handle EtherCAT packet, but failed.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 09:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204069#M10107</guid>
      <dc:creator>BigOrangecat</dc:creator>
      <dc:date>2020-12-24T09:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DPDK l3fwd problem</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204795#M10120</link>
      <description>&lt;P&gt;l3fwd, as it's name suggests, uses L3 headers to make forwarding decisions.&lt;BR /&gt;The L3 protocols it supports are IPv4 and IPv6. This software is not suited for&lt;BR /&gt;handling other types of protocols, such as ARP, which is not strictly L3 or&lt;BR /&gt;EtherCAT which is L2. If you wish to handle other types of protocols, you &lt;BR /&gt;probably need to look at different DPDK applications or even create your own&lt;BR /&gt;from scratch. Everything depends on how you actually want to handle your ingress&lt;BR /&gt;egress traffic. If the task is just to make the node transparent to ARP,&lt;BR /&gt;you can take a look at l2fwd. As of EtherCAT, there is no support to it in &lt;BR /&gt;DPDK or LSDK at all.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 07:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204795#M10120</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-12-29T07:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DPDK l3fwd problem</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204819#M10121</link>
      <description>&lt;P&gt;&lt;EM&gt;thank you for your answering&lt;/EM&gt;&lt;SPAN&gt;&amp;nbsp;of the question.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Dec 2020 08:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LS1046A-DPDK-l3fwd-problem/m-p/1204819#M10121</guid>
      <dc:creator>BigOrangecat</dc:creator>
      <dc:date>2020-12-29T08:20:30Z</dc:date>
    </item>
  </channel>
</rss>