<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: SC16IS760 maximum baud rate</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1203208#M10095</link>
    <description>&lt;P&gt;I see. Thanks!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question on the load capacitance for the crystal. In figure 16, it shows that the two load capacitors used are different in the capacitance. However, in the past I typically see crystals with two capacitors with equivalent value.&lt;/P&gt;&lt;P&gt;Any particular reason to use two different capacitors in figure 16? Thanks!&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Dec 2020 19:06:55 GMT</pubDate>
    <dc:creator>Martin10</dc:creator>
    <dc:date>2020-12-22T19:06:55Z</dc:date>
    <item>
      <title>SC16IS760 maximum baud rate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1201588#M10072</link>
      <description>&lt;P&gt;Dear Sir/Madam,&lt;/P&gt;&lt;P&gt;Based on the datasheet of &lt;SPAN class="lia-link-navigation child-thread lia-link-disabled"&gt;SC16IS760, it states that the maximum baud rate this part can generate is 5 Mbps.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-link-navigation child-thread lia-link-disabled"&gt;Also, from the datasheet I can see that the baud rate can be generated from the external crystal. I am wondering if there is a maximum crystal frequency that&amp;nbsp;SC16IS760 can interface with? Would it work well with a 32 MHz crystal, just for example?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-link-navigation child-thread lia-link-disabled"&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Dec 2020 05:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1201588#M10072</guid>
      <dc:creator>Martin10</dc:creator>
      <dc:date>2020-12-18T05:34:06Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS760 maximum baud rate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1202701#M10085</link>
      <description>&lt;P&gt;Please see datasheet page50-Table 38. fXTAL dynamic characteristics&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 02:46:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1202701#M10085</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-12-22T02:46:31Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS760 maximum baud rate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1203208#M10095</link>
      <description>&lt;P&gt;I see. Thanks!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question on the load capacitance for the crystal. In figure 16, it shows that the two load capacitors used are different in the capacitance. However, in the past I typically see crystals with two capacitors with equivalent value.&lt;/P&gt;&lt;P&gt;Any particular reason to use two different capacitors in figure 16? Thanks!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Dec 2020 19:06:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1203208#M10095</guid>
      <dc:creator>Martin10</dc:creator>
      <dc:date>2020-12-22T19:06:55Z</dc:date>
    </item>
    <item>
      <title>Re: SC16IS760 maximum baud rate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1205699#M10139</link>
      <description>&lt;P&gt;No particular reason,you can use the same value.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jan 2021 02:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SC16IS760-maximum-baud-rate/m-p/1205699#M10139</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-01-04T02:22:09Z</dc:date>
    </item>
  </channel>
</rss>