<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPWM control using QN9080</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197199#M10024</link>
    <description>&lt;P&gt;I'm using the QN9080.&lt;BR /&gt;I'm generating PWM using SCTimer.&lt;BR /&gt;I want to create a function that stops and regenerates the PWM when a specific command is received.&lt;BR /&gt;In the example of scimer_simple_pwm, the PWM generation has been tested, but the PWM output does not stop.&lt;BR /&gt;I thought using the SCTIMER_StopTimer function would stop the output at zero, but I guess not.&lt;/P&gt;&lt;P&gt;How can I turn the PWM output on and off?&lt;/P&gt;</description>
    <pubDate>Thu, 10 Dec 2020 07:58:21 GMT</pubDate>
    <dc:creator>roem</dc:creator>
    <dc:date>2020-12-10T07:58:21Z</dc:date>
    <item>
      <title>PWM control using QN9080</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197199#M10024</link>
      <description>&lt;P&gt;I'm using the QN9080.&lt;BR /&gt;I'm generating PWM using SCTimer.&lt;BR /&gt;I want to create a function that stops and regenerates the PWM when a specific command is received.&lt;BR /&gt;In the example of scimer_simple_pwm, the PWM generation has been tested, but the PWM output does not stop.&lt;BR /&gt;I thought using the SCTIMER_StopTimer function would stop the output at zero, but I guess not.&lt;/P&gt;&lt;P&gt;How can I turn the PWM output on and off?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 07:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197199#M10024</guid>
      <dc:creator>roem</dc:creator>
      <dc:date>2020-12-10T07:58:21Z</dc:date>
    </item>
    <item>
      <title>Re: PWM control using QN9080</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197270#M10025</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;How did you test? If possible, make some screenshots about your code.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 08:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197270#M10025</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-12-10T08:43:10Z</dc:date>
    </item>
    <item>
      <title>Re: PWM control using QN9080</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197682#M10028</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="roem_0-1607643325702.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132404i1957C7B4CADAD8E2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="roem_0-1607643325702.png" alt="roem_0-1607643325702.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Here's the code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thx.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 23:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197682#M10028</guid>
      <dc:creator>roem</dc:creator>
      <dc:date>2020-12-10T23:36:12Z</dc:date>
    </item>
    <item>
      <title>Re: PWM control using QN9080</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197729#M10030</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The red circle code, you needn't put it in the function. deinit should be removed. &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="3.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/132408i89E3ECE1BBE4122B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="3.png" alt="3.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 02:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197729#M10030</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-12-11T02:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: PWM control using QN9080</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197795#M10031</link>
      <description>&lt;P&gt;Thank you for your answer.&lt;BR /&gt;So the PWM is output with the StartTimer, and the PWM is stopped with the StopTimer?&lt;BR /&gt;The red circle code was in that function, so it didn't stop?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 03:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197795#M10031</guid>
      <dc:creator>roem</dc:creator>
      <dc:date>2020-12-11T03:38:47Z</dc:date>
    </item>
    <item>
      <title>Re: PWM control using QN9080</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197868#M10032</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Some material for you to refer.&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Send-a-command-string-through-Bluetooth-to-control-a-QN908X/ta-p/1114885" target="_self"&gt;Send a command string through Bluetooth to control a QN908X three-phase PWM.&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The attachment is the code.&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 11 Dec 2020 06:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-control-using-QN9080/m-p/1197868#M10032</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-12-11T06:17:30Z</dc:date>
    </item>
  </channel>
</rss>