<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSS Security &amp; MaintenanceのトピックAccount setup and login method using vsftp (331,530 error)</title>
    <link>https://community.nxp.com/t5/OSS-Security-Maintenance/Account-setup-and-login-method-using-vsftp-331-530-error/m-p/1941655#M26</link>
    <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20240828_095653.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295654i40E709D4288486A9/image-size/large?v=v2&amp;amp;px=999" alt="20240828_095653.png" title="20240828_095653.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20240828_100224_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295656iFB6D6267CF8B96BF/image-size/large?v=v2&amp;amp;px=999" alt="20240828_100224_1.jpg" title="20240828_100224_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20240828_100224_2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295655iBB4F36BFA37716A2/image-size/large?v=v2&amp;amp;px=999" alt="20240828_100224_2.jpg" title="20240828_100224_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I only want to log in to the account with the password set in vsftpd.conf, so I set it as follows.&lt;/P&gt;&lt;P&gt;After setting up, when I enter the account and password set in the Filezila program, 331 and 530 errors occur.&lt;/P&gt;&lt;P&gt;The password has been tried in various formats, and the same problem occurs even if the password is entered correctly.&lt;/P&gt;&lt;P&gt;The linux kernel version is 6.1.22, and the vsftpd version is 3.0.5.&lt;BR /&gt;The architecture is arm64. (Operating System: NXP i.MX Release Distro 6.1-mickledore (mickledore))&lt;/P&gt;&lt;P&gt;The account was made with the "passwd ftp" command.&lt;/P&gt;&lt;P&gt;Is there a way to solve this problem?&lt;/P&gt;</description>
    <pubDate>Wed, 28 Aug 2024 01:39:15 GMT</pubDate>
    <dc:creator>hsj</dc:creator>
    <dc:date>2024-08-28T01:39:15Z</dc:date>
    <item>
      <title>Account setup and login method using vsftp (331,530 error)</title>
      <link>https://community.nxp.com/t5/OSS-Security-Maintenance/Account-setup-and-login-method-using-vsftp-331-530-error/m-p/1941655#M26</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20240828_095653.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295654i40E709D4288486A9/image-size/large?v=v2&amp;amp;px=999" alt="20240828_095653.png" title="20240828_095653.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20240828_100224_1.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295656iFB6D6267CF8B96BF/image-size/large?v=v2&amp;amp;px=999" alt="20240828_100224_1.jpg" title="20240828_100224_1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="20240828_100224_2.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295655iBB4F36BFA37716A2/image-size/large?v=v2&amp;amp;px=999" alt="20240828_100224_2.jpg" title="20240828_100224_2.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I only want to log in to the account with the password set in vsftpd.conf, so I set it as follows.&lt;/P&gt;&lt;P&gt;After setting up, when I enter the account and password set in the Filezila program, 331 and 530 errors occur.&lt;/P&gt;&lt;P&gt;The password has been tried in various formats, and the same problem occurs even if the password is entered correctly.&lt;/P&gt;&lt;P&gt;The linux kernel version is 6.1.22, and the vsftpd version is 3.0.5.&lt;BR /&gt;The architecture is arm64. (Operating System: NXP i.MX Release Distro 6.1-mickledore (mickledore))&lt;/P&gt;&lt;P&gt;The account was made with the "passwd ftp" command.&lt;/P&gt;&lt;P&gt;Is there a way to solve this problem?&lt;/P&gt;</description>
      <pubDate>Wed, 28 Aug 2024 01:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSS-Security-Maintenance/Account-setup-and-login-method-using-vsftp-331-530-error/m-p/1941655#M26</guid>
      <dc:creator>hsj</dc:creator>
      <dc:date>2024-08-28T01:39:15Z</dc:date>
    </item>
  </channel>
</rss>