<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックLS1046 Core VDD supply section Power MOSFET issue</title>
    <link>https://community.nxp.com/t5/NXP-Designs/LS1046-Core-VDD-supply-section-Power-MOSFET-issue/m-p/1480597#M983</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have made a LS1046 based SOM using the NXP LS1046 RDB. RDB has used LTC3866 switching regulator to generate core VDD 1.0V&amp;nbsp;@ 20A. The Power MOSFETS used on Top Gate is Infenion BSZ0506NS and Bottom Gate is BSC010NE2LSI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is an package related layout issue on the Top Gate section. Can I use the Bottom Gate N Channel MOSFET (&amp;nbsp;BSC010NE2LSI) at the Top Gate ? The two MOSFETS hae different foot print and My PCB is received with Bottom Gate MOSFET foot print at both locations.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Mon, 27 Jun 2022 12:50:47 GMT</pubDate>
    <dc:creator>SrinivasP</dc:creator>
    <dc:date>2022-06-27T12:50:47Z</dc:date>
    <item>
      <title>LS1046 Core VDD supply section Power MOSFET issue</title>
      <link>https://community.nxp.com/t5/NXP-Designs/LS1046-Core-VDD-supply-section-Power-MOSFET-issue/m-p/1480597#M983</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have made a LS1046 based SOM using the NXP LS1046 RDB. RDB has used LTC3866 switching regulator to generate core VDD 1.0V&amp;nbsp;@ 20A. The Power MOSFETS used on Top Gate is Infenion BSZ0506NS and Bottom Gate is BSC010NE2LSI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is an package related layout issue on the Top Gate section. Can I use the Bottom Gate N Channel MOSFET (&amp;nbsp;BSC010NE2LSI) at the Top Gate ? The two MOSFETS hae different foot print and My PCB is received with Bottom Gate MOSFET foot print at both locations.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Jun 2022 12:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/LS1046-Core-VDD-supply-section-Power-MOSFET-issue/m-p/1480597#M983</guid>
      <dc:creator>SrinivasP</dc:creator>
      <dc:date>2022-06-27T12:50:47Z</dc:date>
    </item>
  </channel>
</rss>