<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックPCA85073A RTC Failure</title>
    <link>https://community.nxp.com/t5/NXP-Designs/PCA85073A-RTC-Failure/m-p/1269609#M893</link>
    <description>&lt;P&gt;&lt;SPAN&gt;We are using PCA85073 together with supercapacitor as a backup supply. During cyclic damp heat test (95% humidity and Temperature 55 Degree) and supercapacitor as a backup supply we observed failure after 12-16 Hrs that is RTC fails to continue. But during external power(%V supply using power supply) RTC works fine.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 28 Apr 2021 10:50:03 GMT</pubDate>
    <dc:creator>vaibhav_waman</dc:creator>
    <dc:date>2021-04-28T10:50:03Z</dc:date>
    <item>
      <title>PCA85073A RTC Failure</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PCA85073A-RTC-Failure/m-p/1269609#M893</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are using PCA85073 together with supercapacitor as a backup supply. During cyclic damp heat test (95% humidity and Temperature 55 Degree) and supercapacitor as a backup supply we observed failure after 12-16 Hrs that is RTC fails to continue. But during external power(%V supply using power supply) RTC works fine.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Apr 2021 10:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PCA85073A-RTC-Failure/m-p/1269609#M893</guid>
      <dc:creator>vaibhav_waman</dc:creator>
      <dc:date>2021-04-28T10:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: PCA85073A RTC Failure</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PCA85073A-RTC-Failure/m-p/1270624#M894</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Vaibhav Waman,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;please see below a reply from a quality engineer I have contacted. Please answer his question.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;DESCRIPTION&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN&gt;We run our moisture resistance stress of the package to JEDEC conditions.&lt;BR /&gt;&lt;BR /&gt;This is 85% RH, 130C for 96 hrs under bias of max operating voltage.&amp;nbsp; The part is validated as passing if it passes the datasheet specification.&lt;BR /&gt;I don’t know the correlation between the customer’s moisture resistance test and the JEDEC standard.&lt;BR /&gt;&lt;BR /&gt;Has the RTC been visually inspected to see if there is any ingression of moisture or contamination?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;With Best Regards,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;Jozef&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 03:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PCA85073A-RTC-Failure/m-p/1270624#M894</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-04-30T03:39:14Z</dc:date>
    </item>
  </channel>
</rss>