<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN5180 EEPROM question in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204012#M818</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; You may refer to an EEPROM data sheet for more details on that. For example,&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/NXH5104.pdf?pspll=1" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/data-sheet/NXH5104.pdf?pspll=1&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This means implicitly that the PN5180 contains this EEPROM ?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Dec 2020 07:03:30 GMT</pubDate>
    <dc:creator>Shio_Tamba</dc:creator>
    <dc:date>2020-12-24T07:03:30Z</dc:date>
    <item>
      <title>PN5180 EEPROM question</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1203329#M816</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a question about the EEPROM in PN5180.&lt;/P&gt;&lt;P&gt;I can find this Q&amp;amp;A about read/write cycle for the EEPROM.&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;A href="https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-Hardware-question/m-p/1097966" target="_blank"&gt;https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-Hardware-question/m-p/1097966&lt;/A&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Q1. I cannot understand the "read/write cycle". The "1 cycle" means only read cycle or only write cycle ?&lt;/P&gt;&lt;P&gt;Q2. I guess that the write cycle occurs when I send the "WRITE_EEPROM", "UPDATE_EEPROM", etc. command to PN5180, and the read cycle occurs when I send the "READ_EEPROM", "RETREVE_RF_CONFIG" etc. command to PN5180. The read/write cycle occurs the other case?&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, if we use the DPC, the register values are from EEPROM when the gear changes. The read cycle occurs in this case?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Dec 2020 02:09:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1203329#M816</guid>
      <dc:creator>Shio_Tamba</dc:creator>
      <dc:date>2020-12-23T02:09:47Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 EEPROM question</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204004#M817</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181696"&gt;@Shio_Tamba&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Q1. I cannot understand the "read/write cycle". The "1 cycle" means only read cycle or only write cycle ?&lt;/P&gt;
&lt;P&gt;- The "read/write cycle" here means the program cycle which including writing and erasing.&lt;/P&gt;
&lt;P&gt;Q2. I guess that the write cycle occurs when I send the "WRITE_EEPROM", "UPDATE_EEPROM", etc. command to PN5180, and the read cycle occurs when I send the "READ_EEPROM", "RETREVE_RF_CONFIG" etc. command to PN5180. The read/write cycle occurs the other case?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For example, if we use the DPC, the register values are from EEPROM when the gear changes. The read cycle occurs in this case?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- Yes, your understanding is correct.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no parameter else other&amp;nbsp;&lt;SPAN style="font-family: inherit;"&gt;than the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-family: inherit;"&gt;data retention time&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="font-family: inherit;"&gt;related with read operation.&amp;nbsp; You may refer to an EEPROM data sheet for more details on that. For example,&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/data-sheet/NXH5104.pdf?pspll=1" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/NXH5104.pdf?pspll=1&lt;/A&gt;&amp;nbsp;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-family: inherit;"&gt;Hope that makes sense,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 06:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204004#M817</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-12-24T06:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 EEPROM question</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204012#M818</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;gt; You may refer to an EEPROM data sheet for more details on that. For example,&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/NXH5104.pdf?pspll=1" target="_blank" rel="nofollow noopener noreferrer"&gt;https://www.nxp.com/docs/en/data-sheet/NXH5104.pdf?pspll=1&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This means implicitly that the PN5180 contains this EEPROM ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 07:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204012#M818</guid>
      <dc:creator>Shio_Tamba</dc:creator>
      <dc:date>2020-12-24T07:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 EEPROM question</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204036#M819</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181696"&gt;@Shio_Tamba&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, you put too much interpretation on my answer. This data sheet is just helpful for you to understand the program cycle as well as the data ret&lt;SPAN&gt;ention time better.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 07:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-EEPROM-question/m-p/1204036#M819</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-12-24T07:53:56Z</dc:date>
    </item>
  </channel>
</rss>