<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Default Configuration for SJA1105TEL Ethernet Switch in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1161373#M772</link>
    <description>&lt;P&gt;Hi Platon,&lt;BR /&gt;&lt;BR /&gt;Thank you for your reply. Where can I find the&amp;nbsp;&lt;SPAN&gt;configuration tool SW package ? Does this require us signing an NDA ?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Arun.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Sep 2020 14:13:36 GMT</pubDate>
    <dc:creator>arun_panangala</dc:creator>
    <dc:date>2020-09-30T14:13:36Z</dc:date>
    <item>
      <title>Default Configuration for SJA1105TEL Ethernet Switch</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1158924#M763</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We are developing a custom hardware solution with the&amp;nbsp;SJA1105TEL which connects a PHY, SBC and a FPGA with RGMII interface. Is there a default configuration provided by NXP that we can upload&amp;nbsp; using the &lt;SPAN&gt;sja1105-tool to get the system running with basic functionality&amp;nbsp;like forwarding packets from the PHY to the SBC ?&lt;BR /&gt;&lt;BR /&gt;Kind Regards&lt;BR /&gt;Arun.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 00:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1158924#M763</guid>
      <dc:creator>arun_panangala</dc:creator>
      <dc:date>2020-09-25T00:14:33Z</dc:date>
    </item>
    <item>
      <title>Re: Default Configuration for SJA1105TEL Ethernet Switch</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1161356#M771</link>
      <description>&lt;P&gt;If on your board all switch connections are RGMII, you can start with /example_configs/pyScripts/create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000.py. Thie file is part of the configuration tool SW package. Details can be found in AH1601&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 13:20:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1161356#M771</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-09-30T13:20:33Z</dc:date>
    </item>
    <item>
      <title>Re: Default Configuration for SJA1105TEL Ethernet Switch</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1161373#M772</link>
      <description>&lt;P&gt;Hi Platon,&lt;BR /&gt;&lt;BR /&gt;Thank you for your reply. Where can I find the&amp;nbsp;&lt;SPAN&gt;configuration tool SW package ? Does this require us signing an NDA ?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Arun.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Sep 2020 14:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1161373#M772</guid>
      <dc:creator>arun_panangala</dc:creator>
      <dc:date>2020-09-30T14:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: Default Configuration for SJA1105TEL Ethernet Switch</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1162177#M776</link>
      <description>&lt;P&gt;This tool is part of &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SJA1105TJPABP" target="_blank" rel="noopener"&gt;SJA1105 Application Board Package 1.4&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Platon&lt;/P&gt;</description>
      <pubDate>Fri, 02 Oct 2020 08:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1162177#M776</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-10-02T08:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: Default Configuration for SJA1105TEL Ethernet Switch</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1162736#M777</link>
      <description>&lt;P&gt;Hi Platon,&lt;BR /&gt;&lt;BR /&gt;I have found the Python file you were referring to:&amp;nbsp; /example_configs/pyScripts/create_config_Basic_L2_Switching_No_Priority_Queue_RGMII_1000.py.&lt;BR /&gt;&lt;BR /&gt;I found out that the following parameters depend on the board layout, so they need to be changed for my application:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;xMII_MODE[0..4]&lt;/LI&gt;&lt;LI&gt;PHY_MAC[0..4]&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Is there any other board-specific (e.g. port dependent) register I need to change? If I just changed the above two parameters, would it work?&lt;/P&gt;&lt;P&gt;The block diagram of my system is available below. I just want my three devices (i.e. Jetson Xavier AGX, ethernet jack, and the other MAC device) to communicate.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Hermawan Mulyono&lt;BR /&gt;&lt;BR /&gt;EDIT: I should have replied to &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt; 's post directly, but I could not post two messages in an hour.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="blockdiagram.JPG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126735i93E6F9CC93F076E1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="blockdiagram.JPG" alt="blockdiagram.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 06:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1162736#M777</guid>
      <dc:creator>hmulyono</dc:creator>
      <dc:date>2020-10-05T06:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: Default Configuration for SJA1105TEL Ethernet Switch</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1163284#M782</link>
      <description>&lt;P&gt;To be clear: there is no one-fits-all configuration for SJA1105 switch. What&amp;nbsp; &lt;SPAN class="uiOutputText"&gt;example_configs/pyScripts&lt;/SPAN&gt;/ directory provides, is a set of more-or-less typical configurations for a&amp;nbsp; reference. You can start with the one that is close to what your board needs, but it cannot save you reading the documentation. Refer to &lt;A href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=AH1601&amp;amp;location=null" target="_self"&gt;AH1601&lt;/A&gt; for&amp;nbsp; board and interface specific parts of the switch configuration.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Oct 2020 08:38:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Default-Configuration-for-SJA1105TEL-Ethernet-Switch/m-p/1163284#M782</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2020-10-06T08:38:04Z</dc:date>
    </item>
  </channel>
</rss>