<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 Re: Flexcan Example Rx Not Working</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Flexcan-Example-Rx-Not-Working/m-p/1147684#M708</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;by default a RX MB is configured to receive standard ID 0x511 or 0x555 if NODE_A is defined or not&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So do you send from other node message with right ID?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Fri, 04 Sep 2020 11:31:47 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2020-09-04T11:31:47Z</dc:date>
    <item>
      <title>Flexcan Example Rx Not Working</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Flexcan-Example-Rx-Not-Working/m-p/1138280#M706</link>
      <description>&lt;P&gt;I created a SDK project from examples (S32K144_Project_FlexCan).&amp;nbsp; I could not make the CAN receive work. I can transmit CAN messages though.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 18:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Flexcan-Example-Rx-Not-Working/m-p/1138280#M706</guid>
      <dc:creator>alexbueno929</dc:creator>
      <dc:date>2020-09-03T18:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan Example Rx Not Working</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Flexcan-Example-Rx-Not-Working/m-p/1147684#M708</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;by default a RX MB is configured to receive standard ID 0x511 or 0x555 if NODE_A is defined or not&lt;/P&gt;&lt;DIV class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So do you send from other node message with right ID?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2020 11:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Flexcan-Example-Rx-Not-Working/m-p/1147684#M708</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2020-09-04T11:31:47Z</dc:date>
    </item>
  </channel>
</rss>