<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 Re: Upgrading MCUXpresso results in a larger compiled code</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Upgrading-MCUXpresso-results-in-a-larger-compiled-code/m-p/1080287#M601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="293135" data-username="vithalkamat" href="https://community.nxp.com/people/vithalkamat"&gt;Vithal Kamat&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;"Would it be possible to ensure that the libraries that each of the IDE uses is the same"&lt;/P&gt;&lt;P&gt;Sorry , it seems no, IDE development team choose new LIB as a whole consideration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jul 2020 07:56:34 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2020-07-27T07:56:34Z</dc:date>
    <item>
      <title>Upgrading MCUXpresso results in a larger compiled code</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Upgrading-MCUXpresso-results-in-a-larger-compiled-code/m-p/1080286#M600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just upgraded my MCUXpresso IDE from 10.2.1 Build 795 to the latest 11.2.0 Build 4120.&lt;/P&gt;&lt;P&gt;However, I have noticed that the LPC802 project that I am recompiling with the new IDE results in a larger code size.With the older IDE version, the hex code size was 0x2300 while with the new IDE it has increased to 0x23a0.&lt;/P&gt;&lt;P&gt;The MCU C Compiler Optimization is the same, namely, None (-O0).&lt;/P&gt;&lt;P&gt;I have tried with the latest version of the IDE both on an Ubuntu as well on a Windows OS. Both consistently compile and output hex code of size&amp;nbsp; 0x23a0.&amp;nbsp;&lt;/P&gt;&lt;P&gt;On close comparison of the two disassembly codes, I observe that the new compiler with IDE 11.2.0, is inserting extra nop instructions 46 c0 ( 2 bytes) at certain addresses in the code. So also the size of&amp;nbsp;__vfprintf&amp;nbsp; and other such libraries are also different.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Would it be possible to ensure that the libraries that each of the IDE uses is the same so that we can have consistent code size?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 10:48:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Upgrading-MCUXpresso-results-in-a-larger-compiled-code/m-p/1080286#M600</guid>
      <dc:creator>vithalkamat</dc:creator>
      <dc:date>2020-07-23T10:48:16Z</dc:date>
    </item>
    <item>
      <title>Re: Upgrading MCUXpresso results in a larger compiled code</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Upgrading-MCUXpresso-results-in-a-larger-compiled-code/m-p/1080287#M601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="293135" data-username="vithalkamat" href="https://community.nxp.com/people/vithalkamat"&gt;Vithal Kamat&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;"Would it be possible to ensure that the libraries that each of the IDE uses is the same"&lt;/P&gt;&lt;P&gt;Sorry , it seems no, IDE development team choose new LIB as a whole consideration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2020 07:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Upgrading-MCUXpresso-results-in-a-larger-compiled-code/m-p/1080287#M601</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2020-07-27T07:56:34Z</dc:date>
    </item>
  </channel>
</rss>