<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP DesignsのトピックRe: PN5180 with linux_libnfc-nci or WRITE_NDEF</title>
    <link>https://community.nxp.com/t5/NXP-Designs/PN5180-with-linux-libnfc-nci-or-WRITE-NDEF/m-p/948468#M60</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you tell me where is the error? Or add "printf" for debugging to narrow down the issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Oct 2019 09:05:09 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2019-10-31T09:05:09Z</dc:date>
    <item>
      <title>PN5180 with linux_libnfc-nci or WRITE_NDEF</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-with-linux-libnfc-nci-or-WRITE-NDEF/m-p/948467#M59</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use the PN5180 high-power NFC reader on Raspbian. This reader uses SPI. Whenever I try to send continuous NDEF messages (an image split into 200-byte parts) I always end up getting "Internal Error" (defined within the ph-status.h file) after a random number of messages sent. I am not sure if it's the receiver's fault or the reader's fault. Sometimes adding long 1-second delays helps it, but it's not guaranteed, and it takes sometimes 10 seconds to timeout on a send. I need the process to finish within 5 seconds maximum.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;library that comes with it (SW3693) doesn't have any good examples for writing NDEF messages, it only has a bunch of "forum" examples, discovery loops, and edge-case solutions. The only one that is of any use is Example3_NFCForum, and I had to heavily modify that to do a simple NDEF message write using &lt;STRONG&gt;phalTop_WriteNdef&lt;/STRONG&gt;().&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before this I had used the PN7150 (lower power) also on Raspbian. This library uses I2C instead of SPI, but it never once dropped a packet or got an internal error. It also has multiple actually useful examples, including a tag-write_example, which was what I modeled my image transfer program after.&lt;/P&gt;&lt;P&gt;I'd much prefer to use this library instead of the PN5180 libraries, or at least have an example that works consistently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone direct me to the correct resources?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Oct 2019 23:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-with-linux-libnfc-nci-or-WRITE-NDEF/m-p/948467#M59</guid>
      <dc:creator>riley_baird</dc:creator>
      <dc:date>2019-10-21T23:56:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 with linux_libnfc-nci or WRITE_NDEF</title>
      <link>https://community.nxp.com/t5/NXP-Designs/PN5180-with-linux-libnfc-nci-or-WRITE-NDEF/m-p/948468#M60</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you tell me where is the error? Or add "printf" for debugging to narrow down the issue?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2019 09:05:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/PN5180-with-linux-libnfc-nci-or-WRITE-NDEF/m-p/948468#M60</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2019-10-31T09:05:09Z</dc:date>
    </item>
  </channel>
</rss>