<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SJA1105 can be used between two mcu？ in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069215#M536</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SJA1105 is configured via SPI, so it should be configured by the controller with SPI connection to the switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jun 2020 16:21:37 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2020-06-23T16:21:37Z</dc:date>
    <item>
      <title>SJA1105 can be used between two mcu？</title>
      <link>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069212#M533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My Pcb has two MCU：S32V234 and TC297. If I use a SJA1105 to connect this two mcu, is it OK？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jun 2020 07:23:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069212#M533</guid>
      <dc:creator>caolejun</dc:creator>
      <dc:date>2020-06-19T07:23:55Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105 can be used between two mcu？</title>
      <link>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069213#M534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 06:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069213#M534</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-06-22T06:57:50Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105 can be used between two mcu？</title>
      <link>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069214#M535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Bulat Karymov!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I chose TC297 to control SJA1105 by SPI,then in my code:&lt;/P&gt;&lt;P&gt;1. Should TC297 initialize SJA1105 first?&lt;/P&gt;&lt;P&gt;2. S32v need initialize SJA1105?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2020 00:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069214#M535</guid>
      <dc:creator>caolejun</dc:creator>
      <dc:date>2020-06-23T00:35:26Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1105 can be used between two mcu？</title>
      <link>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069215#M536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The SJA1105 is configured via SPI, so it should be configured by the controller with SPI connection to the switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2020 16:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/SJA1105-can-be-used-between-two-mcu/m-p/1069215#M536</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-06-23T16:21:37Z</dc:date>
    </item>
  </channel>
</rss>