<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NXP Designs中的主题 Download to EVK 1170</title>
    <link>https://community.nxp.com/t5/NXP-Designs/Download-to-EVK-1170/m-p/1066942#M517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have this issue with nxp board EVK 1170 using IAR IDE to program it.&lt;/P&gt;&lt;P&gt;When debugging my code I got a crash but I could not download anymore the program inside the card since the error was rectified. It ends up with this error in the debug windows :&amp;nbsp;"Reading memory at 0x20241400 failed while verifying download". Can anyone help me please ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Aug 2020 15:52:28 GMT</pubDate>
    <dc:creator>cedric-tunde_no</dc:creator>
    <dc:date>2020-08-05T15:52:28Z</dc:date>
    <item>
      <title>Download to EVK 1170</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Download-to-EVK-1170/m-p/1066942#M517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have this issue with nxp board EVK 1170 using IAR IDE to program it.&lt;/P&gt;&lt;P&gt;When debugging my code I got a crash but I could not download anymore the program inside the card since the error was rectified. It ends up with this error in the debug windows :&amp;nbsp;"Reading memory at 0x20241400 failed while verifying download". Can anyone help me please ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2020 15:52:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Download-to-EVK-1170/m-p/1066942#M517</guid>
      <dc:creator>cedric-tunde_no</dc:creator>
      <dc:date>2020-08-05T15:52:28Z</dc:date>
    </item>
    <item>
      <title>Re: Download to EVK 1170</title>
      <link>https://community.nxp.com/t5/NXP-Designs/Download-to-EVK-1170/m-p/1066943#M518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Cedric,&lt;/P&gt;&lt;P&gt;I hope you are great, could you please contact your NXP products distributor for this issue?&lt;BR /&gt;Have a great day,&lt;BR /&gt;Fabian&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2020 15:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/Download-to-EVK-1170/m-p/1066943#M518</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2020-08-06T15:50:48Z</dc:date>
    </item>
  </channel>
</rss>