<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC540: Voltage at ADC input before VDD in NXP Designs</title>
    <link>https://community.nxp.com/t5/NXP-Designs/LPC540-Voltage-at-ADC-input-before-VDD/m-p/1051865#M435</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I have a design, where I am trying to measure voltages with a LPC54016.&lt;BR /&gt;One ADC input is a voltage, that will be on an ADC pin, before the MCU gets powered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have VCC_5V that gets converted into VCC_3V3 with a step down DCDC converter.&lt;BR /&gt;I have 5V going to an ADC input (with a voltage divider, so it is 2.25V at the pin).&lt;BR /&gt;That means, that the 2.25V will be on the ADC pin before 3.3V at the power supply pins.&lt;BR /&gt;&lt;BR /&gt;Can this damage the MCU?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Jana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2020 18:14:20 GMT</pubDate>
    <dc:creator>jana_beck</dc:creator>
    <dc:date>2020-05-06T18:14:20Z</dc:date>
    <item>
      <title>LPC540: Voltage at ADC input before VDD</title>
      <link>https://community.nxp.com/t5/NXP-Designs/LPC540-Voltage-at-ADC-input-before-VDD/m-p/1051865#M435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;I have a design, where I am trying to measure voltages with a LPC54016.&lt;BR /&gt;One ADC input is a voltage, that will be on an ADC pin, before the MCU gets powered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have VCC_5V that gets converted into VCC_3V3 with a step down DCDC converter.&lt;BR /&gt;I have 5V going to an ADC input (with a voltage divider, so it is 2.25V at the pin).&lt;BR /&gt;That means, that the 2.25V will be on the ADC pin before 3.3V at the power supply pins.&lt;BR /&gt;&lt;BR /&gt;Can this damage the MCU?&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Jana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 18:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/LPC540-Voltage-at-ADC-input-before-VDD/m-p/1051865#M435</guid>
      <dc:creator>jana_beck</dc:creator>
      <dc:date>2020-05-06T18:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC540: Voltage at ADC input before VDD</title>
      <link>https://community.nxp.com/t5/NXP-Designs/LPC540-Voltage-at-ADC-input-before-VDD/m-p/1051866#M436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;STRONG&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="356719" data-username="jana.beck@verkada.com" href="https://community.nxp.com/people/jana.beck@verkada.com"&gt;Jana Beck&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Due to the internal circuitry, it is not recommendable to apply voltage to the pins before powering the VDD, this may cause you trouble with the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I apologize for the inconvenience this is causing you, if you have more questions do not hesitate to ask me. &lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2020 18:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NXP-Designs/LPC540-Voltage-at-ADC-input-before-VDD/m-p/1051866#M436</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-05-08T18:59:25Z</dc:date>
    </item>
  </channel>
</rss>